Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Unable to boot from SD card 14.4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 667 views
  • Users 0 members are here
Related

Unable to boot from SD card 14.4

e14 Contributor
e14 Contributor over 13 years ago

Hello i am trying to boot from SD card.
I have a working SDK project and bitfile from EDK, which can be properly transmitted to the Zedboard and i am able to run the software.

Then i pressed: Xilinx Tools --> Create Zynq Boot Image

In the following Windows  i added the FSBL elf file, which i had to download from a Tutorial as in 14.4 it is not possible to create a new project with xilinx templates!

Then I added the bitfile for the system and finally the elf file from my application. It is the elf file from the Debug Folder of my Application.

Then a *.Bin and *.MSC file is generated.

I copied the Bin file to the SD Card and started the board. No blue LED turns on, which indicates that even the bitfile isnt loaded. So anyone got an idead?

I tried to follow the Zedboard boot guide for 14.1.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    It's definitely possible to create a FSBL using SDK 14.4.  File > New > Application Project then select C with a standalone OS and click Next to bring up a list of the available templates.

    I think the FSBL doesn't depend on the HW configuration, but try to generate your own just in case.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Thanks i got the Templates and also working from SD Card

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    add i uart in pl exported to sdk and made boot image .
    copy boot image in sd card .but the board is not booting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi mukesh

    Could you be a bit more descriptive please.

    What have you put in the boot image?
    Are you trying to boot Linux or a standalone program?
    What else have you got on the SD card?
    Does the blue LED which indicates the PL has been programmed come on?

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi !!
    I'm using the SDK 14.6 (32bits). I created the FSBL and created Boot image then copy BOOT.BIN to SD card. The FSBL doesn't work Blue LED doesn't turn on. But if i replace the new FSBL with the old one from example, the BOOT.BIN work normally. Anyone give me what wrong is it ? Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello,
    I have a similar problem, I have followed the Zynq-Intro labs and creating a bare metal application and some logic on PL. Everything works fine using JTAG.

    I want to boot my application from SD. I have created the FSBL proyect and the BOOT.BIN file but the blue led doesnu00B4t turn on ... any suggestions pls??!

    Thanks in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello,

    May be from the other side of the process, but I am following the steps to bring FMCOMMS1 + Zedboard from H/W reference design and face similar problems using Vivado 2014.2 64bit on Linux.

    I have bit file that I can use to configure PL through SDK->Xilinx Tools->Program FPGA

    The led LD12 becomes lit.  I have created bin and mcs files - but non of them configure the PL.  I have tried using QSPI (SDK->Xilinx Tools->Program Flash) with both mcs and bin files - that didn't succeed. Same with bin file when booting from SD card.  But if I place bin file from provided SD card - the system brings up.

    Pavel