Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Communication between Linux and FPGA
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 363 subscribers
  • Views 942 views
  • Users 0 members are here
Related

Communication between Linux and FPGA

e14 Contributor
e14 Contributor over 13 years ago

Hello everybody! I followed zynqgeek's useful tutorial on how to create custom peripheral using PL and to communicate using a bare metal application. Now I'm trying to do something more, like creating a linux application to read/write the registers in the peripheral. My questions are:

1) I'd like to use mmap to map the device into user space, such that is possible to read and write data. Is this correct?

2) Assuming point 1 is ok, is possible to send an interrupt from FPGA to Linux application to inform that some data are available?

3) Do I have to create a Bare Metal application able to communicate to Linux app? If yes, how can the communication be established? If no, I think that can be used mmap + interrupt..

4) Finally I'd like to run the application after the kernel has been loaded. Should I include u-boot.elf during the creation of BOOT.BIN? I tried to include "system.bit", "my_application.elf" and "zynq_fsbl_0.elf", but it seems that Linux is not loaded..

Waiting for your answers!!

Thank you,

sticken

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I thought it was passible to run Linux AND a bare metal application by creating BOOT.BIN from u-boot.elf, my_app.elf, fsbl.elf and sys.bit. Am I wrong?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I thought it was passible to run Linux AND a bare metal application by creating BOOT.BIN from u-boot.elf, my_app.elf, fsbl.elf and sys.bit. Am I wrong?