Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development UART application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 365 subscribers
  • Views 2936 views
  • Users 0 members are here
Related

UART application

e14 Contributor
e14 Contributor over 12 years ago

Dear all,
I'm new to Microzed and I need to use UART communication for my project. I need to get data using the UART and I cannot found any tutorial that helps me to set the UART. I already found example from Xilinx but it is not working. Any idea where I can get the tutorial to setting the UART?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Which UART are you trying to use, UART1 which is connected by default to the USB-UART device, or UART0 which is not connected by default? Exactly what are you attempting to do? And which Xilinx example is not working.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Which UART are you trying to use, UART1 which is connected by default to the USB-UART device, or UART0 which is not connected by default? Exactly what are you attempting to do? And which Xilinx example is not working.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I have already connected the UART0 and UART1 to the Pmod port and didn't have any problem with it. Also I have already test hello world for both of them. The problem occurs when I tried get data from other device with UART and use them as an interrupt. thx alot.








    * @file xuartlite_intr_example.c
    *
    * This file contains a design example using the UartLite driver (XUartLite) and
    * hardware device using the interrupt mode.
    *
    * @note
    *
    * The user must provide a physical loopback such that data which is
    * transmitted will be received.
    *
    * MODIFICATION HISTORY:
    * <pre>
    * Ver   Who  Date     Changes
    * ----- ---- -------- -----------------------------------------------
    * 1.00a jhl  02/13/02 First release
    * 1.00b rpm  10/01/03 Made XIntc declaration global
    * 1.00b sv   06/09/05 Minor changes to comply to Doxygen and coding guidelines
    * 2.00a ktn  10/20/09 Updated to use HAL Processor APIs and minor changes
    *              for coding guidelnes.
    * </pre>
    ******************************************************************************/

    /***************************** Include Files *********************************/

    #include "xparameters.h"
    #include "xuartlite.h"
    #include "xintc.h"
    #include "xil_exception.h"

    /************************** Constant Definitions *****************************/

    /*
    * The following constants map to the XPAR parameters created in the
    * xparameters.h file. They are defined here such that a user can easily
    * change all the needed parameters in one place.
    */
    #define UARTLITE_DEVICE_ID      XPAR_UARTLITE_0_DEVICE_ID
    #define INTC_DEVICE_ID          XPAR_INTC_0_DEVICE_ID
    #define UARTLITE_INT_IRQ_ID     XPAR_INTC_0_UARTLITE_1_VEC_ID

    /*
    * The following constant controls the length of the buffers to be sent
    * and received with the UartLite device.
    */
    #define TEST_BUFFER_SIZE        1


    /**************************** Type Definitions *******************************/


    /***************** Macros (Inline Functions) Definitions *********************/


    /************************** Function Prototypes ******************************/

    int UartLiteIntrExample(u16 DeviceId);

    int SetupInterruptSystem(XUartLite *UartLitePtr);

    void SendHandler(void *CallBackRef, unsigned int EventData);

    void RecvHandler(void *CallBackRef, unsigned int EventData);

    /************************** Variable Definitions *****************************/

    XUartLite UartLite;            /* The instance of the UartLite Device */

    XIntc InterruptController;     /* The instance of the Interrupt Controller */

    /*
    * The following variables are shared between non-interrupt processing and
    * interrupt processing such that they must be global.
    */

    /*
    * The following buffers are used in this example to send and receive data
    * with the UartLite.
    */
    u8 SendBuffer[TEST_BUFFER_SIZE];
    u8 ReceiveBuffer[TEST_BUFFER_SIZE];

    /*
    * The following counters are used to determine when the entire buffer has
    * been sent and received.
    */
    static volatile int TotalReceivedCount;
    static volatile int TotalSentCount;


    /******************************************************************************/
    /**
    *
    * Main function to call the UartLite interrupt example.
    *
    * @param    None
    *
    * @return    XST_SUCCESS if successful, XST_FAILURE if unsuccessful
    *
    * @note        None
    *
    *******************************************************************************/
    int main(void)
    {
        int Status;

        /*
         * Run the UartLite Interrupt example, specify the Device ID that is
         * generated in xparameters.h.
         */
        Status = UartLiteIntrExample(UARTLITE_DEVICE_ID);
        if (Status != XST_SUCCESS) {
            return XST_FAILURE;
        }

        return XST_SUCCESS;
    }

    /****************************************************************************/
    /**
    *
    * This function does a minimal test on the UartLite device and driver as a
    * design example. The purpose of this function is to illustrate
    * how to use the XUartLite component.
    *
    * This function sends data and expects to receive the same data through the
    * UartLite. The user must provide a physical loopback such that data which is
    * transmitted will be received.
    *
    * This function uses interrupt driver mode of the UartLite device. The calls
    * to the UartLite driver in the handlers should only use the non-blocking
    * calls.
    *
    * @param    DeviceId is the Device ID of the UartLite Device and is the
    *        XPAR_<uartlite_instance>_DEVICE_ID value from xparameters.h.
    *
    * @return    XST_SUCCESS if successful, otherwise XST_FAILURE.
    *
    * @note
    *
    * This function contains an infinite loop such that if interrupts are not
    * working it may never return.
    *
    ****************************************************************************/
    int UartLiteIntrExample(u16 DeviceId)
    {
        int Status;
        int Index;

        /*
         * Initialize the UartLite driver so that it's ready to use.
         */
        Status = XUartLite_Initialize(&UartLite, DeviceId);
        if (Status != XST_SUCCESS) {
            return XST_FAILURE;
        }

        /*
         * Perform a self-test to ensure that the hardware was built correctly.
         */
        Status = XUartLite_SelfTest(&UartLite);
        if (Status != XST_SUCCESS) {
            return XST_FAILURE;
        }

        /*
         * Connect the UartLite to the interrupt subsystem such that interrupts can
         * occur. This function is application specific.
         */
        Status = SetupInterruptSystem(&UartLite);
        if (Status != XST_SUCCESS) {
            return XST_FAILURE;
        }

        /*
         * Setup the handlers for the UartLite that will be called from the
         * interrupt context when data has been sent and received, specify a
         * pointer to the UartLite driver instance as the callback reference so
         * that the handlers are able to access the instance data.
         */
        XUartLite_SetSendHandler(&UartLite, SendHandler, &UartLite);
        XUartLite_SetRecvHandler(&UartLite, RecvHandler, &UartLite);

        /*
         * Enable the interrupt of the UartLite so that interrupts will occur.
         */
        XUartLite_EnableInterrupt(&UartLite);
        xil_printf("run");
        /*
         * Initialize the send buffer bytes with a pattern to send and the
         * the receive buffer bytes to zero to allow the receive data to be
         * verified.
         */
    //    for (Index = 0; Index < TEST_BUFFER_SIZE; Index++) {
    //        SendBuffer[Index] = Index;
    //        ReceiveBuffer[Index] = 0;
    //    }
    //
    //    /*
    //     * Start receiving data before sending it since there is a loopback.
    //     */
    //    XUartLite_Recv(&UartLite, ReceiveBuffer, TEST_BUFFER_SIZE);
    //
    //    /*
    //     * Send the buffer using the UartLite.
    //     */
    //    XUartLite_Send(&UartLite, SendBuffer, TEST_BUFFER_SIZE);
    //
    //    /*
    //     * Wait for the entire buffer to be received, letting the interrupt
    //     * processing work in the background, this function may get locked
    //     * up in this loop if the interrupts are not working correctly.
    //     */
    //    while ((TotalReceivedCount != TEST_BUFFER_SIZE) ||
    //        (TotalSentCount != TEST_BUFFER_SIZE)) {
    //    }
    //
    //    /*
    //     * Verify the entire receive buffer was successfully received.
    //     */
    //    for (Index = 0; Index < TEST_BUFFER_SIZE; Index++) {
    //        if (ReceiveBuffer[Index] != SendBuffer[Index]) {
    //            return XST_FAILURE;
    //        }
    //    }
    while(1);

        return XST_SUCCESS;
    }

    /*****************************************************************************/
    /**
    *
    * This function is the handler which performs processing to send data to the
    * UartLite. It is called from an interrupt context such that the amount of
    * processing performed should be minimized. It is called when the transmit
    * FIFO of the UartLite is empty and more data can be sent through the UartLite.
    *
    * This handler provides an example of how to handle data for the UartLite,
    * but is application specific.
    *
    * @param    CallBackRef contains a callback reference from the driver.
    *        In this case it is the instance pointer for the UartLite driver.
    * @param    EventData contains the number of bytes sent or received for sent
    *        and receive events.
    *
    * @return    None.
    *
    * @note        None.
    *
    ****************************************************************************/
    void SendHandler(void *CallBackRef, unsigned int EventData)
    {
        TotalSentCount = EventData;
        print("send");
    }

    /****************************************************************************/
    /**
    *
    * This function is the handler which performs processing to receive data from
    * the UartLite. It is called from an interrupt context such that the amount of
    * processing performed should be minimized.  It is called data is present in
    * the receive FIFO of the UartLite such that the data can be retrieved from
    * the UartLite. The size of the data present in the FIFO is not known when
    * this function is called.
    *
    * This handler provides an example of how to handle data for the UartLite,
    * but is application specific.
    *
    * @param    CallBackRef contains a callback reference from the driver, in
    *        this case it is the instance pointer for the UartLite driver.
    * @param    EventData contains the number of bytes sent or received for sent
    *        and receive events.
    *
    * @return    None.
    *
    * @note        None.
    *
    ****************************************************************************/
    void RecvHandler(void *CallBackRef, unsigned int EventData)
    {
        TotalReceivedCount = EventData;
        xil_printf("recv");
    }

    /****************************************************************************/
    /**
    *
    * This function setups the interrupt system such that interrupts can occur
    * for the UartLite device. This function is application specific since the
    * actual system may or may not have an interrupt controller. The UartLite
    * could be directly connected to a processor without an interrupt controller.
    * The user should modify this function to fit the application.
    *
    * @param    UartLitePtr contains a pointer to the instance of the UartLite
    *           component which is going to be connected to the interrupt
    *           controller.
    *
    * @return   XST_SUCCESS if successful, otherwise XST_FAILURE.
    *
    * @note     None.
    *
    ****************************************************************************/
    int SetupInterruptSystem(XUartLite *UartLitePtr)
    {

        int Status;


        /*
         * Initialize the interrupt controller driver so that it is ready to
         * use.
         */
        Status = XIntc_Initialize(&InterruptController, INTC_DEVICE_ID);
        if (Status != XST_SUCCESS) {
            return XST_FAILURE;
        }


        /*
         * Connect a device driver handler that will be called when an interrupt
         * for the device occurs, the device driver handler performs the
         * specific interrupt processing for the device.
         */
        Status = XIntc_Connect(&InterruptController, UARTLITE_INT_IRQ_ID,
                   (XInterruptHandler)XUartLite_InterruptHandler,
                   (void *)UartLitePtr);
        if (Status != XST_SUCCESS) {
            return XST_FAILURE;
        }

        /*
         * Start the interrupt controller such that interrupts are enabled for
         * all devices that cause interrupts, specific real mode so that
         * the UartLite can cause interrupts through the interrupt controller.
         */
        Status = XIntc_Start(&InterruptController, XIN_REAL_MODE);
        if (Status != XST_SUCCESS) {
            return XST_FAILURE;
        }

        /*
         * Enable the interrupt for the UartLite device.
         */
        XIntc_Enable(&InterruptController, UARTLITE_INT_IRQ_ID);

        /*
         * Initialize the exception table.
         */
        Xil_ExceptionInit();

        /*
         * Register the interrupt controller handler with the exception table.
         */
        Xil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT,
                 (Xil_ExceptionHandler)XIntc_InterruptHandler,
                 &InterruptController);

        /*
         * Enable exceptions.
         */
        Xil_ExceptionEnable();

        return XST_SUCCESS;
    }