Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development zedboard ethernet udp communication
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 366 subscribers
  • Views 4037 views
  • Users 0 members are here
Related

zedboard ethernet udp communication

e14 Contributor
e14 Contributor over 10 years ago

Hello

I´m just playing with ethernet with zedboard. I made simple design with only PS part of Zynq and reworked SDK lwip raw tcp echo example to udp. Everything works fine but I would like to ask some questions.

Performance:

I have measured transmit output with Jperf (GUI version of iperf utility). UDP payload size was 500B with achieved circa 400Mbit/s and for 1000B payload I got around 700Mbit/s bandwidth performance. Bigger payload per datagram is irrelevant for me because of app layer protocol what I'm gonna use.

In XAPP1026 document there is the chapter about measured performance (page 23 - lwip performance). As you can see...about 900Mbit/s can be achieved with raw TCP (!!!) on the board ZC702.

Did I overlook something? ZC702 have same cpu (666MHz) like zedboard and similar PHY ethernet chip (marvell).

Here is sample of my code:

void myudp_client_init(void)
{
    ip_addr_t DestIPaddr;
    err_t err;
    upcb = udp_new();
    if (upcb!=NULL)
    {
        IP4_ADDR( &DestIPaddr, DEST_IP_ADDR0, DEST_IP_ADDR1, DEST_IP_ADDR2, DEST_IP_ADDR3 );
        err= udp_connect(upcb, &DestIPaddr, UDP_SERVER_PORT);
        if (err == ERR_OK)
        {
            /* Set a receive callback */
            udp_recv(upcb, udp_receive_callback, NULL);
        }
    }
}

static void myudp_client_send(void)
{
    struct pbuf *p;
    static int counter = 0;
    sprintf((char*)data, "counter>%d", counter++);   //for evaluation of received datagrams
     p = pbuf_alloc(PBUF_TRANSPORT,PAYLOAD_SIZE, PBUF_POOL);
    if (p != NULL)
    {
        pbuf_take(p, (char*)data, PAYLOAD_SIZE);  //PAYLOAD_SIZE tried from 200B to 1000B
        udp_send(upcb, p);
        pbuf_free(p);
    }
}

I just call myudp_client_send() while button is pushed. Received datagrams are checked in Wireshark.

 

General question about lwip raw mode:

While I was reading various documentation and example codes of RAW mode for different platforms (Atmel, NXP, STM32...) I always find necessity of calling sys_check_timeouts function in while(1) next to variation of function ethernetif_input (it's called xemacif_input in Xilinx lwip port ). Why is it not in xilinx LWIP examples? Are timers timeouts handled implicitly?

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 9 years ago in reply to janani.subraveti@gmail.com +1
    Hi, Have you tried the lwIP Demo Application template in SDK? Compare it to what you currently have. --Josh http://microzed.org/content/udp-frames-zedboard
Parents
  • drhatch
    0 drhatch over 8 years ago

    I have created a system that uses UDP to transmit and receive data. It transmits a small UDP packet every 0.5 seconds, and receives UDP packets. You can modify it as needed for your application.

    The project does not do anything with the UDP data payload it receives -- it just tosses the data. You can easily insert your application code to do something with it.

    I have posted the project (along with instructions) on Github here: https://github.com/delhatch/Zynq_UDP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drhatch
    0 drhatch over 8 years ago

    I have created a system that uses UDP to transmit and receive data. It transmits a small UDP packet every 0.5 seconds, and receives UDP packets. You can modify it as needed for your application.

    The project does not do anything with the UDP data payload it receives -- it just tosses the data. You can easily insert your application code to do something with it.

    I have posted the project (along with instructions) on Github here: https://github.com/delhatch/Zynq_UDP