Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development FSBL 192KB limit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 868 views
  • Users 0 members are here
Related

FSBL 192KB limit

e14 Contributor
e14 Contributor over 9 years ago

According to the documentation, there is a 192 KB limit on the size of the FSBL (or at least the size which can be loaded into on-chip memor, "The size of the FSBL loaded into OCM is limited to 192 kilobyte").

Unfortunately we need to add some code into the FSBL which pushes the size beyond this limit.

What is the proper workaround so you can utilize the full 256 KB in the FSBL?

Has anyone done this?

I can think of a few hypothetical solutions, but none are very appealing:

1. Make a relocatable library which gets loaded into RAM by the FSBL. (This would have a lot of nasty details, including that entry points would keep changing on each compile. There's no DLL infrastructure to help.)

2. Make a really tiny FSBL that loads our full FSBL.

Is it possible to exceed the 192 KB with code which is not critical to the inital startup tasks?

Thanks for all help!

Stuart

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Thanks for the link. It might just work for what I need. Unfortunately,  can't get the example FSBL_XIP project to build. I'm getting a linker error. Can you please see if it builds on your setup? I am using the 2016.2 version SDK. I'm getting this error, which should hopefully be obvious

    make: *** No rule to make target `C:/Temp/xip/workspace/system_top_wrapper_hw_platform_0/ps7_init.c', needed by `src/ps7_init.o'.  Stop.
     
    I have rebuilt the BSP, etc. to no avail. Thanks again!
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Thanks for the link. It might just work for what I need. Unfortunately,  can't get the example FSBL_XIP project to build. I'm getting a linker error. Can you please see if it builds on your setup? I am using the 2016.2 version SDK. I'm getting this error, which should hopefully be obvious

    make: *** No rule to make target `C:/Temp/xip/workspace/system_top_wrapper_hw_platform_0/ps7_init.c', needed by `src/ps7_init.o'.  Stop.
     
    I have rebuilt the BSP, etc. to no avail. Thanks again!