Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development u-boot for the avnet ultrazedev board via tftp PHY issue/driver issue(s)u
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 363 subscribers
  • Views 954 views
  • Users 0 members are here
  • ultrazed-ev
  • xilinx zynq
  • u-boot
Related

u-boot for the avnet ultrazedev board via tftp PHY issue/driver issue(s)u

pe_in_al
pe_in_al over 4 years ago

I downloaded and built the u-boot-xlnx.git repo, for the avnet ultrazedev board to try to tftp bin files to boot. I am getting the following boot log error messages and need help understanding and resolving the issues.

The issues reported in the boot log are 1)

"ZYNQ GEM: ff0e0000, mdio bus ff0e0000, phyaddr 9, interface rgmii-id

zynq_gem ethernet@ff0e0000: Failed to read eth PHY id, err: -2

2) "No match for driver 'soc_xilinx_zynqmp'

Some drivers were not found"

I built the u-boot project with the following cmds/procedure:

{

In order to configure Ethernet Phy,

Modify git/u-boot-xlnx/arch/arm/dts/avnet-ultrazedev-som-v1.0.dtsi, line 47.

Change: reg = <0>; to: reg = <9>;

}

export CROSS_COMPILE=/rtems/6/bin/aarch64-rtems6-

export DEVICE_TREE=avnet-ultrazedev-cc-v1.0-ultrazedev-som-v1.0

make

bootgen -arch zynqmp -image console.bif -0 /media/calvertpt/ZED_BOOT/BOOT.bin -w on

I should mention that this procedure was previously run successfully by colleagues a ffew years ago. I am guessing that the u-boot-xlnx.git project has had many changes in the interim.

The goal is to have uboot boot new kernel/app image files via tftp to avoid wear/ttear on hardware with uSD card operations, and to speed-up development.