Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zynq FSBL is unable to Load BOOT.bin from user selected EMMC offset sector (partition)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 362 subscribers
  • Views 1844 views
  • Users 0 members are here
  • qspi
  • BootROM
  • EMMC Partitions
  • fsbl
  • zynq-7000
  • linux
Related

Zynq FSBL is unable to Load BOOT.bin from user selected EMMC offset sector (partition)

adielement
adielement over 1 year ago

I am working on Zynq-7030 custom board, (software: Vivado 2019.1 → SDK 2019.1).

I have successfully accessed emmc (mmc1 in my case). Created partitions and made understanding of all emmc related commands. My board has two boot modes. One is for SD card and other is QSPI boot.

To load images from EMMC, I need to store bootloader at QSPI (since boot mode is QSPI), so that bootloader boots first and then proceeds to other images loading, that are placed at emmc.

I want to separately load boot.bin, kernel image, dtb and rootfs for each partition of emmc, based on whatever user selects at bootup. In simple words, there should be a user code that asks from user to select the partition to boot from. Say partition 3 is selected, the boot.bin , kernel image, dtb and rootfs corresponding that partition 3 will be booted up and others will not be booted.

I did research on this and found that BootROM allows FSBL to boot from QSPI to OCM. Now I am stuck in customizing FSBL to take user input and then load corresponding images. I made a simple design in Vivado and enabled only EMMC (mmc1/ sd1) and disabled SD (mmc0/sd0) then generated fsbl.elf from SDK. The fsbl.elf is generated by default method, so it does not take user input and then can load corresponding images according to that user input.

I need way out for this. I have beginner level expertise in embedded C so I need help in how to read the offset sector of EMMC to laod BOOT.bin (that was stored using dd command in the EMMC).

Is my understanding of this approach is correct or I need to adapt alternate for this? If it is correct then I will appreciate help in FSBL code customization. 

  • Sign in to reply
  • Cancel

Top Replies

  • tony56887
    tony56887 over 1 year ago in reply to adielement +1
    Primary boot from QSPI with only fsbl, which then hands off to boot from eMMC as secondary boot with full image. Sounds like you have this understood and I also believe this part is achievable. But what…
  • adielement
    0 adielement over 1 year ago

    Can anyone please help me with this. I am stuck in it for many days.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • adielement
    0 adielement over 1 year ago in reply to adielement

    tony56887  do you have any idea on this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tony56887
    0 tony56887 over 1 year ago in reply to adielement

    Primary boot from QSPI with only fsbl, which then hands off to boot from eMMC as secondary boot with full image. Sounds like you have this understood and I also believe this part is achievable.

    But what you need is user prompt and the ability to select which image/partition to load out of multiple partitions on the eMMC? This seems more advanced, and is not provided easily as default functionality by xilinx that i'm aware of. If it's possible you would need to customize your fsbl. I would recommend asking about this on the Xilinx forums.