Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development MicroZed + Yocto : with official "microzed-zynq7" machine, U-Boot does not start from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1862 views
  • Users 0 members are here
Related

MicroZed + Yocto : with official "microzed-zynq7" machine, U-Boot does not start from SD card

gsavaton
gsavaton over 7 years ago

I am building a Yocto Linux image for the MicroZed using the official meta-xilinx layer (Yocto branch "rocko" + meta-xilinx layer with branch "rel-v2018.3").

 

Using MACHINE = "microzed-zynq7" in my local.conf generates an image that fails to boot from SD card:

  • At startup, the blue LED indicates that the PL is configured.
  • The USB-UART port does not output anything.

 

As a workaround, I have created a custom machine configuration based on the official microzed-zynq7.conf with the following modifications:

 

# Use the ZedBoard configuration for U-Boot instead of MicroZed
UBOOT_MACHINE = "zynq_zed_config"

# Keep the device tree of the MicroZed KERNEL_DEVICETREE = "zynq-microzed.dtb"

# Enable the "u-boot-xlnx" recipe (with U-Boot 2018.3)
# instead of the "u-boot" recipe (that provides U-Boot 2017.09).
PREFERRED_PROVIDER_virtual/bootloader = "u-boot-xlnx"

The bootloader generated with this machine definition works correctly and I get a fully working Linux system.

 

In both attempts, the u-boot.elf file from the Yocto build is added to the same bitstream and FSBL generated by Vivado + SDK using the officiel MicroZed board files.

  • Do you know why the microzed-zynq7 machine definition does not generate a working bootloader in my case?
  • Do you think my workaround is safe to use? Should I try something else?
  • Sign in to reply
  • Cancel
Parents
  • dexterous.me82
    dexterous.me82 over 6 years ago

    I tried the same. I have the microzed zynqboard from AVNET.

     

    Next, I have opened xilinx sdk to create fsbl project.

    Next, I have created the bootimage using -

    fsbl image and the uboot.elf generated from the yocto.

     

    However, when I have put this boot.bin, I get the following error.

    I have added debug info for fsbl too. I have tried adding even the dtb file but it didn't help.

    Do I need to rename the file before adding that in the xilinx sdk?

    Does it have any sequence like fsbl first then uboot.elf and then dtb file?

    What am I missing here, please help?

     

     

     

    Xilinx First Stage Boot Loader

    Release 2018.1  Feb 12 2020-16:06:04

    Devcfg driver initialized

    Silicon Version 3.1

    Boot mode is SD

    SD: rc= 0

    SD Init Done

    Flash Base Address: 0xE0100000

    Reboot status register: 0x60600000

    Multiboot Register: 0x0000C000

    Image Start Address: 0x00000000

    Partition Header Offset:0x00000C80

    Partition Count: 2

    Partition Number: 1

    Header Dump

    Image Word Len: 0x0002184D

    Data Word Len: 0x0002184D

    Partition Word Len:0x0002184D

    Load Addr: 0x04000000

    Exec Addr: 0x04000000

    Partition Start: 0x000075D0

    Partition Attr: 0x00000010

    Partition Checksum Offset: 0x00000000

    Section Count: 0x00000001

    Checksum: 0xF7F93EE7

    Application

    Handoff Address: 0x04000000

    In FsblHookBeforeHandoff function

    SUCCESSFUL_HANDOFF

    FSBL Status = 0x1

    No valid device tree binary found - please append one to U-Boot binary, use u-boot-dtb.bin or define CONFIG_OF_EMBED. For sandbox, use -d <file.dtb>

    initcall sequence 0405f82c failed at call 04055fc8 (err=-1)

    ### ERROR ### Please RESET the board ###

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 6 years ago in reply to dexterous.me82

    We at Avnet don't normally do our Linux development with a native yocto flow, so this isn't something we can support.  We use Xilinx PetaLinux.  Think of PetaLinux as a productivity layer between you and yocto "under the covers".  That said, I do not know what is defined in the "microzed-zynq7" machine.

     

    Your best bet may be to start with something known-good like our posted BSPs for the MicroZed:

    MicroZed

    We have BSPs for most recent versions of PetaLinux.

     

    Consult Xilinx UG1144 for how to "install" the BSP:

    https://www.xilinx.com/support/documentation/sw_manuals/xilinx2019_1/ug1144-petalinux-tools-reference-guide.pdf

     

    Cheers,

    Tom

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • narrucmot
    narrucmot over 6 years ago in reply to dexterous.me82

    We at Avnet don't normally do our Linux development with a native yocto flow, so this isn't something we can support.  We use Xilinx PetaLinux.  Think of PetaLinux as a productivity layer between you and yocto "under the covers".  That said, I do not know what is defined in the "microzed-zynq7" machine.

     

    Your best bet may be to start with something known-good like our posted BSPs for the MicroZed:

    MicroZed

    We have BSPs for most recent versions of PetaLinux.

     

    Consult Xilinx UG1144 for how to "install" the BSP:

    https://www.xilinx.com/support/documentation/sw_manuals/xilinx2019_1/ug1144-petalinux-tools-reference-guide.pdf

     

    Cheers,

    Tom

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dexterous.me82
    dexterous.me82 over 6 years ago in reply to narrucmot

    My basic question is let say I want to just build u-boot for microzed-zynq7 board. how can I do so?

    I don't want to use petalinux or yocto. I just want some plain steps that will work and will generate the correct u-boot.elf.

    Basically, the basic make command to generate the u-boot.elf. From where I should clone the u-boot code and next from where I

    should download the cross compiler/sdk to build the u-boot code.