Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96 V2 hangs at boot, console doesn't print anything, custom Linux, Vivado 2018.3
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 365 subscribers
  • Views 827 views
  • Users 0 members are here
  • ultra96
  • boot from ssd
Related

Ultra96 V2 hangs at boot, console doesn't print anything, custom Linux, Vivado 2018.3

nico_n04
nico_n04 over 7 years ago

I used the SDK to generate the PMUFW, device tree, and FSBL. I added debug mode to FSBL and PMUFW and used UART1.

I generated the BOOT.BIN :

bootgen -image test.bif -arch zynqmp -o BOOT.bin -log info -w

 

I have not issues generating the boot.bin.

The test.bif is structure as follow:

 

//arch =  zynqmp; split = false ; format = BIN

the_ROM_image:

{

     [bootloader, destination_cpu = a53-0]FSBL.elf

     [pmufw_image]PMUFW.elf

     [destination_cpu = pl]example.bit

     [destination_cpu = a53-0, exception_level = el-3, trustzone]bl31.elf

     [destination_cpu = a53-0, exception_level = el-2]u-boot.elf

}

 

I have tried everything and read every manual and document I can find. From my understanding the PMUFW its required for the zcu102 dev board, but maybe it is not required for the Ultra96-V2.

I am using Vivado 2018.3, and I loaded the Board Definition Files from Avnet https://github.com/Avnet/bdf

 

any idea?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    bhfletcher over 7 years ago

    The PMU firmware is not required for simple bare metal stuff. I've seen in work without it. But, it is good practice to use it.

     

    Did you change the STDIN/OUT settings to point to psu_uart1?

     

    How are you connecting to the UART pins on J1?

     

    Have you tried booting via JTAG and was it successful?

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nico_n04
    nico_n04 over 7 years ago in reply to bhfletcher

    I figured it out, I had an issue on the PS configuration . I created a new project and make sure not to touch the default configs for now.

    I tested the bitstream project but making sure I was loading the bitstream over the JTAG. It was getting stuck when loading the bitstream over the JTAG.

     

    thanks, for your help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • nico_n04
    nico_n04 over 7 years ago in reply to bhfletcher

    I figured it out, I had an issue on the PS configuration . I created a new project and make sure not to touch the default configs for now.

    I tested the bitstream project but making sure I was loading the bitstream over the JTAG. It was getting stuck when loading the bitstream over the JTAG.

     

    thanks, for your help