Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96v2 Modprobe wilc3000 failed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 366 subscribers
  • Views 1035 views
  • Users 0 members are here
  • ultra96v2
  • wilc3000
  • ultra96
Related

Ultra96v2 Modprobe wilc3000 failed

thomas-schulik
thomas-schulik over 6 years ago

Hello,

 

I have built a new Petalinux 2018.3 image with the usage of the BSP from https://github.com/Avnet/Ultra96-PYNQ  from image_2.4_v2 and added my own hardware design from Vivado 2018.3.

 

petalinux-config --get-hw-description /path-to-sdk-folder

 

When I have booted Petalinux successfully, I would like to connect to the WiFi and I initially executed following command:

 

modprobe wilc-sdio

 

After this I get the response:

 

[   62.466155] wifi_pm : 0

[   62.468637] wifi_pm : 1

[   62.471309] wilc_sdio mmc1:0001:1: Driver Initializing success

root@sensors96b:~# [   62.693564] WILC POWER UP

[   62.696202] wilc_sdio mmc1:0001:1: SDIO speed: 50000000

[   62.701659] wilc_sdio mmc1:0001:1: chipid 003000d0

[   62.708144] wilc_sdio mmc1:0001:1: Direct firmware load for mchp/wilc3000_wifi_firmware.bin failed with error -2

[   62.718326] wilc_sdio mmc1:0001:1: wilc_sdio_disable_interrupt

[   62.742056] power up request for already powered up source Wifi

[   62.747999] Device already up. request source is Wifi

[   62.754776] wilc_sdio mmc1:0001:1: Direct firmware load for mchp/wilc3000_wifi_firmware.bin failed with error -2

[   62.764959] wilc_sdio mmc1:0001:1: wilc_sdio_disable_interrupt

 

What is wrong with my wilc3000 firmware or the connection to the wilc3000 module?

Why the firmware can't be loaded successfully?

 

In the attachment you can find a complete UART Trace from the startup sequence.

 

Regards

Attachments:
UART_Trace_Ultra96_StartUp.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • clem57
    clem57 over 6 years ago

    Refer porting guide and then install the wifi firmware.bin to /lib/firmware.

     

    If you are using petalinux then create a recipe to copy the firmware to rootfs.

     

    DESCRIPTION = "Firmware binaries for use with Microchip ATWILC1003" SECTION = "libs" LICENSE = "MIT" LIC_FILES_CHKSUM = "file://${COMMON_LICENSE_DIR}/MIT;md5=0835ade698e0bcf8506ecda2f7b4f302"  SRC_URI = " \ file://wilc3000_wifi_firmware.bin \ "  S = "${WORKDIR}"  PROVIDES += "wilc3000-firmware" RPROVIDES_${PN} += "wilc3000-firmware"  do_install() { install -d ${D}${base_libdir}/firmware cp -a --no-preserve=ownership ${S}/wilc3000_wifi_firmware.bin ${D}${base_libdir}/firmware/ }  FILES_${PN} = "${base_libdir}/firmware/*"  # Inhibit warnings about files being stripped INSANE_SKIP_${PN} = "ldflags" INHIBIT_PACKAGE_DEBUG_SPLIT = "1" INHIBIT_PACKAGE_STRIP = "1"  # These libraries shouldn't get installed in world builds unless something # explicitly depends upon them. EXCLUDE_FROM_WORLD = "1"

    This is similar to what you need thomas-schulik

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 6 years ago

    Refer porting guide and then install the wifi firmware.bin to /lib/firmware.

     

    If you are using petalinux then create a recipe to copy the firmware to rootfs.

     

    DESCRIPTION = "Firmware binaries for use with Microchip ATWILC1003" SECTION = "libs" LICENSE = "MIT" LIC_FILES_CHKSUM = "file://${COMMON_LICENSE_DIR}/MIT;md5=0835ade698e0bcf8506ecda2f7b4f302"  SRC_URI = " \ file://wilc3000_wifi_firmware.bin \ "  S = "${WORKDIR}"  PROVIDES += "wilc3000-firmware" RPROVIDES_${PN} += "wilc3000-firmware"  do_install() { install -d ${D}${base_libdir}/firmware cp -a --no-preserve=ownership ${S}/wilc3000_wifi_firmware.bin ${D}${base_libdir}/firmware/ }  FILES_${PN} = "${base_libdir}/firmware/*"  # Inhibit warnings about files being stripped INSANE_SKIP_${PN} = "ldflags" INHIBIT_PACKAGE_DEBUG_SPLIT = "1" INHIBIT_PACKAGE_STRIP = "1"  # These libraries shouldn't get installed in world builds unless something # explicitly depends upon them. EXCLUDE_FROM_WORLD = "1"

    This is similar to what you need thomas-schulik

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • thomas-schulik
    thomas-schulik over 6 years ago in reply to clem57

    Hey guys,

     

    I solved the problem in the meanwhile by copying the firmware to the /lib/firmware folder. image

    I was able to set up the SSH scripts and the g_ether connection also, so WiFi and the RNDIS connection is working now.

     

    Thanks for your support.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to thomas-schulik
    I solved the problem in the meanwhile by copying the firmware to the /lib/firmware folder

    Glad it was this simple thomas-schulik

    Clem