Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Diameter of barrel of power plug adapter
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 365 subscribers
  • Views 1958 views
  • Users 0 members are here
  • ultra96
Related

Diameter of barrel of power plug adapter

eduque
eduque over 6 years ago

On the power supply that will plug into the Power Jack (ref des J10) on the Ultra96-V2 board, what is the max diameter of the barrel housing around the plug?  See circled in red.

I only know that the exposed plug itself is 4.7mm x 1.7mm x 10mm from the description.  I can't find a mechanical drawing of the plug assembly from Votoo, and it's important for me to know the barrel dimensions in my application.

image

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy over 6 years ago +2
    Not sure how accurate you need to be, but I have the 4A power supply that has a similar looking barrel plug. The exposed plug measures 4.77mm. The first step up on the barrel is 7.96mm and the max diameter…
  • shabaz
    shabaz over 6 years ago +1
    Hi Emma, It's in the bill-of-materials, the socket is part code PJ1-021-SMT-TR and it's datasheet will have the full details. (it expects a 4.75mm,1.7mm plug, i.e. outer barrel is 4.75mm, inner hole is…
  • ralphjy
    ralphjy over 6 years ago in reply to eduque +1
    Okay, I understand - if you're trying to mount a board on top - the highest features are the two USB connectors but I'm sure you're aware of that (around 3mm higher than the power jack). The 4A supply…
Parents
  • shabaz
    shabaz over 6 years ago

    Hi Emma,

     

    It's in the bill-of-materials, the socket is part code PJ1-021-SMT-TR and it's datasheet will have the full details.

    (it expects a 4.75mm,1.7mm plug, i.e. outer barrel is 4.75mm, inner hole is 1.7mm).

    EDIT: just realized you're looking for the molded plastic shell dimensions. I don't know the answer to that, it is probably unspecified by the manufacturer (and may vary).

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • eduque
    eduque over 6 years ago in reply to shabaz

    Thanks for chiming in, Shabaz!  Yep unfortunately this is the only drawing I was able to find as well.  Since the height of the jack is 6mm, I was interested in how much the plastic shell / barrel extends past the jack when the cable is plugged in.

    If tthe barrel is 9mm dia. (like one of my teammate's power adapters), that means it will extend 1.5mm above the jack's top surface.  This might be ok, but it would be helpful if there was a drawing available from the manufacturer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • eduque
    eduque over 6 years ago in reply to shabaz

    Thanks for chiming in, Shabaz!  Yep unfortunately this is the only drawing I was able to find as well.  Since the height of the jack is 6mm, I was interested in how much the plastic shell / barrel extends past the jack when the cable is plugged in.

    If tthe barrel is 9mm dia. (like one of my teammate's power adapters), that means it will extend 1.5mm above the jack's top surface.  This might be ok, but it would be helpful if there was a drawing available from the manufacturer.