Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design MicroZed board is not powering
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 366 subscribers
  • Views 763 views
  • Users 0 members are here
  • microzed
  • powerup failure
Related

MicroZed board is not powering

correodelusak
correodelusak over 6 years ago

Hi,

 

I just unpacked the microzed (Z10), and does not power up.

I check the USB cable, evetythign is fine... but neither of the LEDs turn on.

 

What is supposed I need to do?

 

Best Regards,

Miguel

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    ctammann over 6 years ago

    Hey Miguel,

     

    Have you tried multiple ports? On some PCs the USB power is shared so you could also have an issue if you have multiple USB devices connected. One quick way to make sure it isn't a port power limit issue would be to use a USB cable and just plug it into a standard USB cell phone charger. If that powers up the board but it doesn't power from the PC there could be an issue with it being properly recognized. If it doesn't power up that can send us down a different diagnosis path.
    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • correodelusak
    correodelusak over 6 years ago in reply to ctammann

    Hi Chris,

     

    Yes, I did. No luck at all.

    I just want to replace the board, as I dont want to spend time finding the root cause of the problem in a board I just unpack from the box.

    I just want a RMA or direct board replacement... but seems the guys from Farnell just direct to this forum.

     

    Out of interest.. I damage the old board I was using, as looks like if you design a daughter card.. the  5V you need to feed into the microzed is effectively 4.3V, due to a lovely diode to "select" between microzed USB power, and 5V power from the connector.

    This should not be a major problem, if the turn_on pin fit into the 1.1V regulator wont be the 5V... as a consequence I blow the 1.1V regulator.

     

    Best Regards,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • correodelusak
    correodelusak over 6 years ago in reply to ctammann

    Hi Chris,

     

    Yes, I did. No luck at all.

    I just want to replace the board, as I dont want to spend time finding the root cause of the problem in a board I just unpack from the box.

    I just want a RMA or direct board replacement... but seems the guys from Farnell just direct to this forum.

     

    Out of interest.. I damage the old board I was using, as looks like if you design a daughter card.. the  5V you need to feed into the microzed is effectively 4.3V, due to a lovely diode to "select" between microzed USB power, and 5V power from the connector.

    This should not be a major problem, if the turn_on pin fit into the 1.1V regulator wont be the 5V... as a consequence I blow the 1.1V regulator.

     

    Best Regards,

    Miguel