Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Cpu speed and Fan control
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 365 subscribers
  • Views 1099 views
  • Users 0 members are here
Related

Cpu speed and Fan control

andycap
andycap over 7 years ago

Hi Guys,

I have just got an ultra96.

 

I thought the main cores were 1.5ghz but they seem to be set to 1.2ghz in cpu_info_max_frequency. Is there a reson for this?

 

Also there doesn't seem to be any fan control, the fan spinning flat out is driving me mad.

Even loading the 4 cores up 100% each my max temp is only 52 so I'm thinking this fan is running a bit fast.

 

Is there any way to enable fan control?

 

Many thanks for any help

 

Andy

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 7 years ago

    The Ultra96 has a -1 speed grade device, which has a max APU frequency of 1.2 GHz. See DS925, Table 28.

    The fan can be controlled via GPIO F4. However, we have not implemented an example for this yet. The idea is to read the temperature and adjust the pulse width on F4. Perhaps someone in the community has already done this and will share.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andycap
    0 andycap over 7 years ago

    Hi Bryan,

     

    Thanks very much for the prompt reply.

    Shame about the speed rating, I was mistaken.

     

    Thanks for the pointer on GPIO F4, I will take a look...

     

    Many thanks

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andycap
    0 andycap over 7 years ago

    Hi Again,

    With the default boot is it possible to get this GPIO into userspace via /sys/class/gpio ?

     

    Thanks

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 7 years ago

    Unfortunately, no. However, it should not be that hard to add. I will request that this get added to the next BSP that gets released.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andycap
    0 andycap over 7 years ago

    Thanks Bryan.

    I was going to look into this aday to see if I can get it going, I will let you know how it goes...