Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Board Definition file bug
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 365 subscribers
  • Views 795 views
  • Users 0 members are here
Related

Board Definition file bug

bhfletcher
bhfletcher over 8 years ago

Be aware that there is a bug in the Board Definition that is embedded in Vivado 2018.1 and 2018.2 for Ultra96 that causes the LPDDR4 to fail at the 1GB mark. We are working on a simple patch now.

 

This does not affect the PetaLinux 2018.2 BSP for Ultra96 that was recently published.

 

Bryan

  • Sign in to reply
  • Cancel
Parents
  • dyessgg
    0 dyessgg over 8 years ago

    I think there might be another defect in the Ultra96 preset.xml file in the GIT repository.

    The 3-pin UART connector is routed to uart_1 at pins MIO 8..9 in hardware.  The preset.xml file shows it at the default location of "MIO 0 .. 1".  Line 97 should be changed to "MIO 8 .. 9". 

    Since MIO 8..9 are used as part of SPI1, SPI 1 will have to be disabled by modifying line 77 to value="0".

    Additionally, the BSP settings should be modified to route stdin and stdout to uart_1 instead of uart_0.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dyessgg
    0 dyessgg over 8 years ago

    I think there might be another defect in the Ultra96 preset.xml file in the GIT repository.

    The 3-pin UART connector is routed to uart_1 at pins MIO 8..9 in hardware.  The preset.xml file shows it at the default location of "MIO 0 .. 1".  Line 97 should be changed to "MIO 8 .. 9". 

    Since MIO 8..9 are used as part of SPI1, SPI 1 will have to be disabled by modifying line 77 to value="0".

    Additionally, the BSP settings should be modified to route stdin and stdout to uart_1 instead of uart_0.