Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Board Definition file bug
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 365 subscribers
  • Views 793 views
  • Users 0 members are here
Related

Board Definition file bug

bhfletcher
bhfletcher over 8 years ago

Be aware that there is a bug in the Board Definition that is embedded in Vivado 2018.1 and 2018.2 for Ultra96 that causes the LPDDR4 to fail at the 1GB mark. We are working on a simple patch now.

 

This does not affect the PetaLinux 2018.2 BSP for Ultra96 that was recently published.

 

Bryan

  • Sign in to reply
  • Cancel
Parents
  • dyessgg
    0 dyessgg over 8 years ago

    I got MIO8..9 from the HW User Guide, rev 1.0, Version 0.9, section 5.7:
    "Ultra96 provides one UART. PS UART1 (MIO8, MIO9) is connected to a 3 pin 2mm header (J6)."

    When I created a Vivado project using the board defaults of MIO0..1, exported to SDK and then created a project based upon that, J6 would not work.

    Apparently, I was a bit hasty in my previous post.  My issue with J6 not working stemmed from the BSP using uart_0 as the default instead of uart_1.  Looks like I was making more than one change at the same time.  Sorry for the confusion.

    Two things from this:
    1. The HW USer Guide is incorrect when it states uart1 is routed via MIO8..9.
    2. The default in Vivado/SDK of using uart_0 instead of uart_1 needs to be overridden.

    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dyessgg
    0 dyessgg over 8 years ago

    I got MIO8..9 from the HW User Guide, rev 1.0, Version 0.9, section 5.7:
    "Ultra96 provides one UART. PS UART1 (MIO8, MIO9) is connected to a 3 pin 2mm header (J6)."

    When I created a Vivado project using the board defaults of MIO0..1, exported to SDK and then created a project based upon that, J6 would not work.

    Apparently, I was a bit hasty in my previous post.  My issue with J6 not working stemmed from the BSP using uart_0 as the default instead of uart_1.  Looks like I was making more than one change at the same time.  Sorry for the confusion.

    Two things from this:
    1. The HW USer Guide is incorrect when it states uart1 is routed via MIO8..9.
    2. The default in Vivado/SDK of using uart_0 instead of uart_1 needs to be overridden.

    Greg