Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Enable the Wi-Fi
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 737 views
  • Users 0 members are here
Related

Enable the Wi-Fi

francocapraro12
francocapraro12 over 7 years ago

Hi guys. (I was trying to find a post, but i couldnt)
Im trying to enable the wi-fi in my own project for the Ultra96 using Petalinux. I did a simple project in Vivado, i made the bitstream and then im trying to enable the Wi-Fi via petalinux-config --get-hw-description=<project.sdk>


IMAGE:https://hackster.imgix.net/uploads/attachments/519102/image_M8BNse8S3V.png?auto=compress%2Cformat&w=1280&h=960&fit=max

image

What i need to make in the Menu?


Im new with the Ultra96 and Petalinux, so if you can explain me in detail i will be better for me.

Thanks for your time !

  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 7 years ago

    When working on a custom Vivado and PetaLinux design for the Ultra96 that also includes WiFi, it may be best to start with the PetaLinux 2018.2 BSP posted on the Xilinx website (you will need to login/register to download this file):

    https://www.xilinx.com/member/forms/download/xef.html?filename=xilinx-ultra96-reva-v2018.2-final.bsp

    The Vivado project is included in the BSP, so you can identify what is required in the PL and PS config for WiFi, etc. and use this as the starting point for your own custom design.  Note that this BSP maps the user UART out to the low-speed mezzanine connector on pins 11 (Tx) and 13 (Rx).  Here is an excerpt from the XDC constraints file for the Vivado hw platform:

    #HD_GPIO_5 on FPGA / Connector pin 13 / UART1_rxd
    set_property PACKAGE_PIN G5 [get_ports UART1_rxd]
    #HD_GPIO_4 on FPGA / Connector pin 11 / UART1_txd
    set_property PACKAGE_PIN F6 [get_ports UART1_txd]
     

    Directions for installing the BSP can be found in Xilinx UG1144:

    https://www.xilinx.com/support/documentation/sw_manuals/xilinx2018_2/ug1144-petalinux-tools-reference-guide.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • francocapraro12
    0 francocapraro12 over 7 years ago in reply to narrucmot

    Thank you for your help ! i will do that ! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • francocapraro12
    0 francocapraro12 over 7 years ago in reply to narrucmot

    Thank you for your help ! i will do that !