Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design buildinging an image on the sd card from my custom design bitstream
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 364 subscribers
  • Views 360 views
  • Users 0 members are here
Related

buildinging an image on the sd card from my custom design bitstream

mdm92
mdm92 over 7 years ago

Hi,

I have previuosly designed a network and implemented it using boot image on zed board. But due to the higher resource demnad for the my upgraded network version I have choosen ultra96.

I desinged it with using  S_axi_HP0 slave interface & connecting it to axi_dma(sg engine disabled). I'm facing two challenges in this case.
first, previously with processing system 7_0 design I had fixed_IO, DDR port as boart preset which i don't have with the zync_ultra_ps_e_0. So after automation I'm not sure about stream out interface.what should i possibly change to make it workin? or should i leave it like it is after automation?

Second, I'm also working on how can i make a boot image from my output bitstream. previously I made it by creating image from sdk(boot.bin and .bif) and loading it into the sd card. I saw an option in ultra 96 website where you have an option using petalinux  "build from source" where they use a design_1_wrapper.bit. I've completed that part and planning to replace with my .bit file. will it work? if not, what should i do to run my .bit using sd card? 

Thank you (I apologize for such a naive and long post)

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 7 years ago

    Have you already looked at the Intro tutorials at http://zedboard.org/support/design/24166/156? Those will walk through the board definition, basic architecture, bare metal test apps, and creating an SD image.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 7 years ago

    Have you already looked at the Intro tutorials at http://zedboard.org/support/design/24166/156? Those will walk through the board definition, basic architecture, bare metal test apps, and creating an SD image.

    Bryan