Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Connect via ssh to Ultra96
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 369 subscribers
  • Views 2875 views
  • Users 0 members are here
Related

Connect via ssh to Ultra96

reis220
reis220 over 7 years ago

Hello everyone,

 

How can i issue some commands to Ultra96 via ssh?

The etc/network/interfaces file has static IP for USB connection:

 

# Ethernet/RNDIS gadget (g_ether)

# ... or on host side, usbnet and random hwaddr

iface usb0 inet static

        address 192.168.7.2

        netmask 255.255.255.0

        network 192.168.7.0

        gateway 192.168.7.1

 

I connect the ethernet cable from my pc to the board's micro-USB upstream port, but when i try to connect using 192.168.7.2 address, it does not connect to the board either. Any ideas what might be wrong with the connection?

  • Sign in to reply
  • Cancel

Top Replies

  • ddbabich
    ddbabich over 7 years ago +2 suggested
    Hi, I'm not sure if you ever solved this, however I had the same issue and followed this Xilinx confluence page under the "Ethernet Gadget" section with success: https://xilinx-wiki.atlassian.net/wiki…
Parents
  • jafoste4
    0 jafoste4 over 7 years ago

    Hi,


    Are you using the out of box image with the board to connect via SSH?

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • reis220
    0 reis220 over 7 years ago in reply to jafoste4

    No, i am using a Petalinux generated image. But the Petalinux configuration doesn't offer other ethernet settings, it only provides "manual" option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • reis220
    0 reis220 over 7 years ago in reply to jafoste4

    No, i am using a Petalinux generated image. But the Petalinux configuration doesn't offer other ethernet settings, it only provides "manual" option.