Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Connect via ssh to Ultra96
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 369 subscribers
  • Views 2867 views
  • Users 0 members are here
Related

Connect via ssh to Ultra96

reis220
reis220 over 7 years ago

Hello everyone,

 

How can i issue some commands to Ultra96 via ssh?

The etc/network/interfaces file has static IP for USB connection:

 

# Ethernet/RNDIS gadget (g_ether)

# ... or on host side, usbnet and random hwaddr

iface usb0 inet static

        address 192.168.7.2

        netmask 255.255.255.0

        network 192.168.7.0

        gateway 192.168.7.1

 

I connect the ethernet cable from my pc to the board's micro-USB upstream port, but when i try to connect using 192.168.7.2 address, it does not connect to the board either. Any ideas what might be wrong with the connection?

  • Sign in to reply
  • Cancel

Top Replies

  • ddbabich
    ddbabich over 7 years ago +2 suggested
    Hi, I'm not sure if you ever solved this, however I had the same issue and followed this Xilinx confluence page under the "Ethernet Gadget" section with success: https://xilinx-wiki.atlassian.net/wiki…
Parents
  • 100sbeaudoin
    0 100sbeaudoin over 7 years ago

    reis220  wrote:

    I connect the ethernet cable from my pc to the board's micro-USB upstream port, but when i try to connect using 192.168.7.2 address, it does not connect to the board either. Any ideas what might be wrong with the connection?

    You mean you have a USB to Ethernet adapter? You HAVE to have one since there is no ethernet jack on the board. And the usb upstream port isn't a usb->ethernet adapter

     

     

     

    When you issue a simple 'petalinux-config' command, in the ethernet section it is normal to only have the 'manual' option. This section lists the physical/genuine/hardware ethernet ports. In vivado, when you use the ultra96 board files and you click apply board presets, it configures the zynqMP ip with the settings found in the board files. Since there is no ethernet jack, the board files do not activate any of the GEM (gigabit ethernet mac). When you export the hardware, that configuration is passed along in the HDF file. When petalinux opens it and parse the hardware configuration, it detects that there is no genuine ethernet support, thats why you don't see the option in the 'petalinux-config' menu. You must probably know that there are several configuration menus in petalinux. The simple 'petalinux-config' is the global one; the "Xilinx" one. The 'petalinux-config -c kernel' is the same as when you do a 'make menuconfig' when compiling the linux kernel, so the petalinux command is in fact a wrapper. It will be in this menu that you will have to find and enable the linux driver for the USB to Ethernet adapter (usb gadget something if i remember, just look it up)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • reis220
    0 reis220 over 7 years ago in reply to 100sbeaudoin

    100sbeaudoin  wrote:

    It will be in this menu that you will have to find and enable the linux driver for the USB to Ethernet adapter (usb gadget something if i remember, just look it up)

    Do i need to enable only on petalinux-config -c kernel? Do i have to modify any device trees too? If yes, what device trees?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100sbeaudoin
    0 100sbeaudoin over 7 years ago in reply to reis220

    Unlike 'platform devices' which  are the ones you  have to make mention in the devce tree because they cant be discovered  at runtime, with usb devices you dont have to mention them in the device tree because they can be discovered at runtime. BUT, in case of usb, for a particular vid:pid, the kernal has to be aware if a driver is available to bind to it. Hence you have to include the driver of the gadget in the config of the kernel. It can either be compiled in the kernel or as a module.

     

     

    And yes obviously you can use the board's usb port to plug the adapter in it. What i meant is that indeed you have to plug an adapter, just pluging a micro usb usb cable from the pc into the micro usb wont work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100sbeaudoin
    0 100sbeaudoin over 7 years ago in reply to 100sbeaudoin

    Only the usb driver in 'petalinux -c kernel' has to be enabled for it to work. I will provide a step by step instructions monday

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • reis220
    0 reis220 over 7 years ago in reply to 100sbeaudoin

    Ok, thank you for your readiness. I'll be waiting for the instructions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • reis220
    0 reis220 over 7 years ago in reply to 100sbeaudoin

    Ok, thank you for your readiness. I'll be waiting for the instructions.