Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96 boots from AVNet's SD card but not mine
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 367 subscribers
  • Views 2211 views
  • Users 0 members are here
  • ultra96
  • boot sequence
  • boot
  • SD card
Related

Ultra96 boots from AVNet's SD card but not mine

rich_dubielzig_rbt
rich_dubielzig_rbt over 7 years ago

I have an Ultra96 that boots to the GUI using the 16Gb SD card that came with the unit.

 

When I create my own SD card that I've populated with my own code.  I cannot boot at all.

 

The red "INIT_B" LED at DS7 stays lit and never switches to the green "DONE" LED at DS6.  I have a USB-to-JTAG/UART Pod for the device, but no serial traffic is detected.

 

However, I don't believe that the board is even attempting to execute my code, because the same behavior is expressed when I copy the contents of the AVNet card's boot partition into my own card's boot partition.  In this situation I would at least expect an attempt to boot, followed by a dump of errors on the monitor due to library mismatches.

 

Questions:

 

1.  What is the meaning of the INIT_B and DONE LEDs?  They are not described in the Ultra96 HW User's Guide.  What software or firmware is responsible for turning on and off the LEDs?

 

2.  Here are the results of fdisk -l run against my own SD card and the AVNet supplied card.  Does anything look wrong in the way it was formatted?

 

 

Stock SD card:

 

root@Ultra96:/var/run/media/mmcblk0p1# fdisk -l /dev/mmcblk0

Disk /dev/mmcblk0: 14.9 GiB, 15931539456 bytes, 31116288 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

Disklabel type: dos

Disk identifier: 0x32f37a38

 

 

Device         Boot   Start      End  Sectors  Size Id Type

/dev/mmcblk0p1 *       2048  2099199  2097152    1G  b W95 FAT32

/dev/mmcblk0p2      2099200 16320511 14221312  6.8G 83 Linux

 

 

My SD card:

 

rich@rich-vbox ~/ultra96/u96_hackster/images/linux $ sudo fdisk -l /dev/sdb

[sudo] password for rich:

Disk /dev/sdb: 59.6 GiB, 64021856256 bytes, 125042688 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

Disklabel type: dos

Disk identifier: 0x01f31e0a

 

 

Device     Boot   Start       End   Sectors  Size Id Type

/dev/sdb1  *       2048   2099199   2097152    1G  b W95 FAT32

/dev/sdb2       2099200 125042687 122943488 58.6G 83 Linux

 

Message was edited by: Rich Dubielzig Added fixed-width formatting to fdisk outputs

  • Sign in to reply
  • Cancel

Top Replies

  • rich_dubielzig_rbt
    rich_dubielzig_rbt over 7 years ago +2 suggested
    The problem was related to my choice of SD card. While I am marking Bryan's answer as correct, I did not go with a Delkin card, but rather a SanDisk Industrial 16Gb card, as that was the exact model that…
  • rich_dubielzig_rbt
    rich_dubielzig_rbt over 7 years ago +1
    A followup to explain how I have attempted to generate my own code. First attempt: Following the instructions posted on 96boards.org, but using Petalinux 2018.3 and the 2018.3 version of the ultra96 BSP…
  • rich_dubielzig_rbt
    0 rich_dubielzig_rbt over 7 years ago

    A followup to explain how I have attempted to generate my own code.

     

    First attempt:

     

    Following the instructions posted on 96boards.org, but using Petalinux 2018.3 and the 2018.3 version of the ultra96 BSP:

     

    https://www.96boards.org/documentation/consumer/ultra96/build/peta-linux.md.html

     

    Second attempt:

     

    Following the instructions given in in the first method of this blog post, but using the 2018.3 versions of Vivado and Xilinx SDK:

     

    https://www.hackster.io/adam-taylor/two-methods-of-building-petalinux-for-the-ultra96-77c8e0

     

    If I built according to the Hackster blog's methods, I should definitely expect serial traffic from the u-boot because psu_uart_1 was specified as stdin/stdout in the petalinux serial settings, correct?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rich_dubielzig_rbt
    0 rich_dubielzig_rbt over 7 years ago in reply to rich_dubielzig_rbt

    I've just attempted a "Factory restore" format of the SD card per the instructions from here:

     

    | Zedboard

     

    I downloaded the SD card image from Linaro and flashed it over the SD card using etcher.  The board still does not boot.

     

    I am using a 64GB Samsung EVO select SD Card.  Is there a maximum SD card size that is supported by the Ultra96?  Do I need one that is exactly 16Gb in size?

     

    -Rich

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 7 years ago in reply to rich_dubielzig_rbt

    I don't have a Zedboard, but there are several possibilities -

    • There could be some incompatibility with Samsung EVO series cards - I've had errors running these cards in Raspberry Pi boards causing intermittent issues (read-only filesystems due to communication errors) and no issues using other brands (Sandisk, Kingmax, Sony, Lexar, Toshiba, etc). It pays to remember that not all cards are equal - in the early days, Raspberry Pi had great issues with certain Class 10 cards ... it often boils down to the way the SD controller is coded as well.
    • There could be a problem with cards of a particular capacity support (e.g. no SDXC, only SDHC).

     

    Perhaps to troubleshoot more, you could:

    • Image your existing working 16GB card and write the image to the 64GB card and try booting from it. If it doesn't boot - it's likely a card compatibility issue (but we don't know if that's size or brand/controller).
    • Try a different branded SDXC (>32GB) card with the same image or try an SDHC card (4-32GB).

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 7 years ago

    I have tested Ultra96 Linux Boot using Delkin Devices 64GB and 128GB microSD cards from their Utility family. Therefore, I know that the hardware can handle the larger sizes. However, we have received other complaints specifically about the Samsung EVO. I'm not sure exactly what the issue is, but others have experienced boot problems with this specific brand of card.

     

    This is a good read -- Storage Insights #1 - Why Not All SD Cards are Created Equal

     

    We specifically chose Delkin Devices to include in our kits because of their "Controlled BOM." See https://www.delkin.com/blog/recognizing-the-importance-of-controlled-boms/  for more information.

     

    If you'd like to give the larger Delkin Devices microSD cards a try, they are available through Newark, with 4, 8, 16, 64, and 128 GB cards currently in stock -- http://www.newark.com/w/search?st=delkin+microSD&product-range=utility-microsd-series&COM=Embedded

     

    If you want an Industrial temperature grade microSD card, then look at Delkin's Utility+ family. Less varieties in stock, but perhaps enough to get you started -- http://www.newark.com/w/search?st=delkin+microSD&product-range=utilitypos-microsd-series&COM=Embedded 

     

    Regarding your previous questions about INIT_B and DONE, the operation of these signals from the MPSoC is defined in the Xilinx configuration documentation for the device -- https://www.xilinx.com/support/documentation/user_guides/ug570-ultrascale-configuration.pdf

     

    • INIT_B:
      • Active-Low FPGA initialization pin or configuration error signal. The FPGA drives this pin Low when the FPGA is in a configuration reset state, when the FPGA is initializing (clearing) its configuration memory, or when the FPGA has detected a configuration error.
    • DONE:
      • A High signal on the DONE pin indicates completion of the configuration sequence. By default, the DONE output is open-drain.

     

    If the INIT_B is lit and the DONE is not, then you have experienced a boot error with the PL, which could definitely be caused by an incompatible microSD card.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rich_dubielzig_rbt
    0 rich_dubielzig_rbt over 7 years ago

    The problem was related to my choice of SD card.

     

    While I am marking Bryan's answer as correct, I did not go with a Delkin card, but rather a SanDisk Industrial 16Gb card, as that was the exact model that shipped with my Ultra96.  Upon flashing the card, I was able to configure and boot the Ultra96.

     

    https://www.newegg.com/Product/Product.aspx?Item=9SIAHRZ8851341

     

     

    Just for posterity and future users, I note that I also tried these two cards, as I could pick them up at Fry's the same day and it turns out that Fry's doesn't carry any SD cards made for "Industrial" use.  Neither worked.

     

    Samsung PRO Endurance 32GB (fail to pass INIT_B state)

     

    Patriot LX 16GB (free space on card smaller than factory reset image size).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 7 years ago in reply to rich_dubielzig_rbt

    Hi,

     

    We actually have a SD card advice document that may be of interest you.

    SD Card Advice V2 for Zynq and Zynq UltraScale+ SoC Products | Zedboard

    Thanks,

    Josh