Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96-v2 USB3.0 issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 366 subscribers
  • Views 1577 views
  • Users 0 members are here
Related

Ultra96-v2 USB3.0 issue

roopasampath
roopasampath over 7 years ago

I have a customer using the Ultra96-v2 board. They want to use the SOM as a USB 3.0 mass storage device to a Windows PC. They are using the standalone baremetal driver usbpsu version 1.4  and xilinx SDK example sb_intr_example.c and along with chapter 9 xusb code. The design compiles successfully and runs and does print messages on JTAG. However, the PC host does not see Ultra96-v2 based usb3.0 device at all. They are using the USB0 controller on the board

 

They have also tried with and with out  "Enable V BUS Port" under USB3.0  in IO configuration of ZYNQMP block using Vivado HLx 2018.2 tools.

 

Any thoughts or direction on how to resolve this would be very much appreciated!

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 7 years ago +1 suggested
    Hi Roopa, Please have your customer look at the following posts to start. https://forums.xilinx.com/t5/Evaluation-Boards/ZCU102-ES2-USB-3-0-Host-mode/td-p/749487 https://xilinx-wiki.atlassian.net/wiki…
  • jafoste4
    0 jafoste4 over 7 years ago

    Hi Roopa,

     

    Please have your customer look at the following posts to start.

     

    https://forums.xilinx.com/t5/Evaluation-Boards/ZCU102-ES2-USB-3-0-Host-mode/td-p/749487

    https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/18842410/Zynq+UltraScale+MPSoC+USB+3.0+Mass+Storage+Device+Class+D…

     

    If they are interested in a Linux Solution.

    https://www.xilinx.com/support/answers/72409.html

     

    Thanks,
    Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • roopasampath
    0 roopasampath over 7 years ago in reply to jafoste4

    Hi Josh,

     

    Thank you. They tried running their design with the 2019.1 SDK and a custom built hdf file on Ultra96v2 board and were able to get the mass Storage USB 3 device is functioning fully.

     

    Regards,

    Roopa