Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Debugging on the Ultra96
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 366 subscribers
  • Views 1616 views
  • Users 0 members are here
Related

Debugging on the Ultra96

jhane
jhane over 7 years ago

Hello,

 

So I've got all the pieces for my design built, bitstream from from Vivado, a Linux image from petalinux for the APUs and a freeRTOS app for RPU0.   However, I'm not clear on how to get it all booted, running and then connecting the debugger to the R5.   What I want to do is boot the APUs and load the PL from the SD card. After that, I want to load and debug the R5 via JTAG.  However, since the dip switches are set to boot from SD this seem to indicate i can't switch them after booting to boot the R5 from jtag.   I haven't tried this yet so I'm curious if this would work.

Or can I create a bif file that will also boot the RPU from the BOOT.BIN on a SD card?   If the dip switches are set to SD, can I still connect to RPU0 via JTAG after boot for debugging?

 

thanks,

jeff

  • Sign in to reply
  • Cancel

Top Replies

  • jhane
    jhane over 7 years ago in reply to clem57 +1
    Hi Clem, That could be one way but really that would have to be a complete act of desperation and really it would only get me part way since in the end I would still need to debug the real system. Some…
  • jhane
    jhane over 6 years ago in reply to bhfletcher +1
    Hi Bryan, Yes, I did eventually find that page and it does explain what is happening. The same thing happen if you connect Vivado to the board after linux has booted. However, before I found that page…
Parents
  • bhfletcher
    0 bhfletcher over 6 years ago

    Regarding your question, "can I create a bif file that will also boot the RPU from the BOOT.BIN on a SD card?"

     

    Yes, that is possible. Here are some resources that walk you through that exercise:

    https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/18842403/Zynq+Ultrascale+MPSoC+Multiboot+and+Fallback

    https://www.xilinx.com/support/documentation/sw_manuals/xilinx2018_3/ug1209-embedded-design-tutorial.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jhane
    0 jhane over 6 years ago in reply to bhfletcher

    Hi,

     

    Thanks, I did figure that out but it really didn't solve anything for my debugging but it's good to know for shipping.

     

    jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jhane
    0 jhane over 6 years ago in reply to bhfletcher

    Hi,

     

    Thanks, I did figure that out but it really didn't solve anything for my debugging but it's good to know for shipping.

     

    jeff