Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design WiFi very slow to connect on boot-up
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 367 subscribers
  • Views 1563 views
  • Users 0 members are here
Related

WiFi very slow to connect on boot-up

jhane
jhane over 6 years ago

Hello,

I've modified my 2018.3 build so that the WiFi will start at boot-up and connect to my hotspot with a static IP.  However, it seem to take a long time, 3-5 minutes, for the network connect to come up.  If I just do /etc/init.d/network restart on the console I can normally connect immediately.    Based on the console logs, the loading of the driver is the last thing to occur before getting a login prompt:

 

[    5.574698] wifi_pm : 0

[    5.577185] wifi_pm : 1

[    5.579987] wilc_sdio mmc1:0001:1: Driver Initializing success

[    5.589445] WILC POWER UP

[    5.592105] wilc_sdio mmc1:0001:1: SDIO speed: 50000000

[    5.598191] wilc_sdio mmc1:0001:1: chipid 003000d0

 

 

Has anybody seen this problem?

 

thanks,

jeff

  • Sign in to reply
  • Cancel

Top Replies

  • zedhed
    zedhed over 6 years ago in reply to jhane +1
    Hi Jeff, What machine are you pinging Ultra96 from? Is it the Ubuntu Desktop? If so, is the ARP cache getting cleared under Ubuntu during the Ultra96 reboot? If so, then Ubuntu will have to resolve the…
Parents
  • clem57
    0 clem57 over 6 years ago

    This is a know bug/feature in Linux. The solution:

     

    Found a solution, it seems that the new kernels are compiled with "Accelerate last non-dyntick-idle CPU's grace periods (RCU_FAST_NO_HZ)" option: Yes

     

    explanation from the Linux kernel source:

    This option causes RCU to attempt to accelerate grace periods
    in order to allow CPUs to enter dynticks-idle state more
    quickly. On the other hand, this option increases the overhead
    of the dynticks-idle checking, particularly on systems with
    large numbers of CPUs.

     

    If you add

    nohz=off

    to the kernel line in grub the "NOHZ local_softirq_pending"  messages don't show up

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to clem57

    A better wording:

    Add nohz=off to the kernel parameters during boot to disable it.

    This option causes RCU to attempt to accelerate grace periods in order to allow CPUs to enter dynticks-idle state more quickly. On the other hand, this option increases the overhead of the dynticks-idle checking, particularly on systems with large numbers of CPUs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 6 years ago in reply to clem57

    A better wording:

    Add nohz=off to the kernel parameters during boot to disable it.

    This option causes RCU to attempt to accelerate grace periods in order to allow CPUs to enter dynticks-idle state more quickly. On the other hand, this option increases the overhead of the dynticks-idle checking, particularly on systems with large numbers of CPUs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 6 years ago in reply to clem57

    But this really a symptom of DHCP from the router being slow!