Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Bluetooth on Ultra96V2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 368 subscribers
  • Views 2081 views
  • Users 0 members are here
Related

Bluetooth on Ultra96V2

mah110mat
mah110mat over 7 years ago

I'm trying to connect a keyboard via bluetooth on Ultra96V2 board.

But it does not work well.

Could anyone give me any advices to connect?

followings are my operations..

 

1. boot a board by Linux from http://avnet.me/ultra96-v2-oob.

2. login by root

3. use a script as blow

  echo BT_POWER_UP > /dev/wilc_bt

  echo BT_DOWNLOAD_FW > /dev/wilc_bt

  echo BT_FW_CHIP_WAKEUP > /dev/wilc_bt

    # after this command, same messages are shown repeatedly that is " [  341.066759] Another device is preventing allow sleep operation. request source is Wifi"

 

  stty -F /dev/ttyS1 115200

  stty -F /dev/ttyS1 crtscts

  hciattach /dev/ttyS1 -t 10 any 115200 noflow nosleep

    # this command looks like work well a moment, but timeout message came up after few seconds.

       [  171.245441] Bluetooth: hci0 command 0x1003 tx timeout

       [  173.261438] Bluetooth: hci0 command 0x1001 tx timeout

       [  175.277387] Bluetooth: hci0 command 0x1009 tx timeout

 

  hciconfig -a

    # this command gives a message but BD Address looks like weird.

      hciconfig -a

      hci0:    Type: Primary  Bus: UART

          BD Address: 00:00:00:00:00:00  ACL MTU: 0:0  SCO MTU: 0:0

          DOWN INIT RUNNING

          RX bytes:0 acl:0 sco:0 events:0 errors:0

          TX bytes:12 acl:0 sco:0 commands:3 errors:0

          Features: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00

          Packet type: DM1 DH1 HV1

          Link policy:

          Link mode: SLAVE ACCEPT

 

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • lightcollector
    lightcollector over 6 years ago in reply to nerdyupdates +1 suggested
    Hi, The commands I show work under PYNQ v2.5 which uses the device uart shown. For the user using a different uart device name that it didn't work I am suspicious that the hardware PS pin configuration…
Parents
  • anantanus
    0 anantanus over 6 years ago

    Hi,

     

    Were you able to solve it?

     

    Can you please share it if you had solved it?

     

    Im facing the same issue

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lightcollector
    0 lightcollector over 6 years ago in reply to anantanus

    Try this:

     

    # Do this only once after board power-up:

    echo BT_POWER_UP > /dev/wilc_bt

    echo BT_DOWNLOAD_FW > /dev/wilc_bt

     

    stty -F /dev/ttyPS1 115200

    # Initialize the device:

    hciattach /dev/ttyPS1 -t 10 any 115200 noflow nosleep

    sleep 1s

    hciconfig hci0 up

    hciconfig hci0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mah110mat
    0 mah110mat over 6 years ago in reply to lightcollector

    Thank you for comments.
    Unfortunately, I can not solve this issue yet.
    I tried following as lightcollector commented.

    before trying, I checked which port connected to the BT module.
    # dmesg|grep ttyPS
    [ 2.515418] ff000000.serial: ttyPS2 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps
    [ 2.519401] ff010000.serial: ttyPS0 at MMIO 0xff010000 (irq = 41, base_baud = 6249999) is a xuartps

    in my environment, it looks like that ttyPS2 is connecting to BT module.

    # echo BT_POWER_UP > /dev/wilc_bt
    [ 72.729601] at_pwr_dev: open()
    [ 72.732708] AT PWR: bt_power_up
    [ 72.735861] Device already up. request source is BT
    [ 72.742316] at_pwr_dev: close()
    # echo BT_DOWNLOAD_FW > /dev/wilc_bt
    [ 74.117535] at_pwr_dev: open()
    [ 74.120598] AT PWR: bt_download_fw
    [ 74.124006] Bluetooth firmware: mchp/wilc3000_ble_firmware.bin
    [ 74.136755] Downloading BT firmware size = 58184 ...
    [ 74.294713] Starting BT firmware
    [ 74.405466] BT Start Succeeded
    [ 74.408555] at_pwr_dev: close()
    # stty -F /dev/ttyPS2 115200
    # hciattach /dev/ttyPS2 -t 10 any 115200 noflow nosleep
    Device setup complete
    [ 100.589430] Bluetooth: hci0 command 0x1003 tx timeout
    [ 102.605462] Bluetooth: hci0 command 0x1001 tx timeout
    [ 104.621462] Bluetooth: hci0 command 0x1009 tx timeout
    # hciconfig hci0
    hci0: Type: Primary Bus: UART
    BD Address: 00:00:00:00:00:00 ACL MTU: 0:0 SCO MTU: 0:0
    DOWN
    RX bytes:0 acl:0 sco:0 events:0 errors:0
    TX bytes:12 acl:0 sco:0 commands:3 errors:0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nerdyupdates
    0 nerdyupdates over 6 years ago in reply to mah110mat

    I am having the same issue. Have you had any luck solving this? I was able to plug in a Cinolink USB-Bluetooth dongle and get it to pair/communicate, but I would prefer to use the built-in Bluetooth to the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lightcollector
    0 lightcollector over 6 years ago in reply to nerdyupdates

    Hi, The commands I show work under PYNQ v2.5 which uses the device uart shown.  For the user using a different uart device name that it didn't work I am suspicious that the hardware PS pin configuration for flow control is not quite right and the wilc3000 cannot communicate after the firmware load or the device tree setting.  On PYNQ I see proper status responses coming back and all is well enough for the next layer of software to work.

     

    Kind regards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nerdyupdates
    0 nerdyupdates over 6 years ago in reply to lightcollector

    That was my fear. Guess it's time to go back and take a look at the hardware configuration.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nerdyupdates
    0 nerdyupdates over 6 years ago in reply to lightcollector

    That was my fear. Guess it's time to go back and take a look at the hardware configuration.