Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design How to fix ramdisk load address (etc.) stopping boot-up of Xen build for 2018.3 on Ultra96v2?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 364 subscribers
  • Views 1340 views
  • Users 0 members are here
Related

How to fix ramdisk load address (etc.) stopping boot-up of Xen build for 2018.3 on Ultra96v2?

granchee
granchee over 6 years ago

Hi all,

 

I have an Avnet Ultra96v2 and a Petalinux Xen Hypervisor build made with the Xilinx 2018.3 SDK and this 2018.3 BSP: http://downloads.element14.com/downloads/zedboard/ultra96/ultra96v2_oob_2018_3.zip

 

Instructions followed to make the Xen build: https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/76677121/Building+Xen+Hypervisor+with+Petalinux+2018.3

 

After petalinux-build and preparing the SD card I power-up the board and stop the autoboot, then follow the steps in the Xilinx document at SD Booting Xen and Dom0 | RootFS mounted on RAM (initrd):

 

ZynqMP> mmc dev 0 &&&& mmcinfo

switch to partitions #0, OK

mmc0 is current device

Device: mmc@ff160000

Manufacturer ID: 3

OEM: 5344

Name: SU32G

Tran Speed: 50000000

Rd Block Len: 512

SD version 3.0

High Capacity: Yes

Capacity: 29.7 GiB

Bus Width: 4-bit

Erase Group Size: 512 Bytes

 

ZynqMP> load mmc 0 1000000 system.dtb &&&& load mmc 0 0x80000 Image

reading system.dtb

54761 bytes read in 21 ms (2.5 MiB/s)

reading Image

15034880 bytes read in 1082 ms (13.3 MiB/s)

 

ZynqMP> fdt addr 1000000

 

ZynqMP> load mmc 0 1030000 xen.ub

reading xen.ub

786832 bytes read in 72 ms (10.4 MiB/s)

 

ZynqMP> load mmc 0 2000000 rootfs.cpio.gz.u-boot

reading rootfs.cpio.gz.u-boot

455152849 bytes read in 32454 ms (13.4 MiB/s)

 

I then do bootm 1030000 2000000 1000000, but it doesn't go well:

 

## Booting kernel from Legacy Image at 01030000 ...

   Image Name:

   Image Type:   AArch64 Linux Kernel Image (uncompressed)

   Data Size:    786768 Bytes = 768.3 KiB

   Load Address: 06000000

   Entry Point:  06000000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 02000000 ...

   Image Name:   petalinux-user-image-ultra96-zyn

   Image Type:   AArch64 Linux RAMDisk Image (uncompressed)

   Data Size:    455152785 Bytes = 434.1 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 01000000

   Booting using the fdt blob at 0x1000000

   Loading Kernel Image ... OK

   Loading Ramdisk to ffffffffecdee000, end 07fff491 ... "Synchronous Abort" handler, esr 0x96000144

ELR:     8001738

LR:      801bd80

x0 : ffffffffecdee000 x1 : 0000000007fff4c0

x2 : 0000000000000040 x3 : 000000000000003f

x4 : 000000002320f491 x5 : 0000000000000000

x6 : 000000007fe6e558 x7 : 000000002320f491

x8 : 000000007dd928f0 x9 : 0000000000000008

x10: 00000000ffffffd8 x11: 000000007ff00000

x12: 000000007fe9ebc8 x13: 000000007dd91a70

x14: ffffffffecdee000 x15: 0000000000000008

x16: 0000000000000002 x17: 0000000007fff491

x18: 000000007dd92de8 x19: 000000001b211491

x20: 0000000008000000 x21: 0000000002000040

x22: 000000007fe9eb28 x23: 000000007fe9eb00

x24: 000000007fe9eaf8 x25: 0000000001030040

x26: 0000000000000000 x27: 0000000000000000

x28: 0000000006000000 x29: 000000007dd92a30

 

Resetting CPU ...

 

resetting ...

Xilinx Zynq MP First Stage Boot Loader

Release 2018.3   Oct  4 2019  -  11:41:21

 

The ramdisk load address looks bad.

 

If so, how and where is it defined?

How to fix it?

 

For the record, if I follow the instructions at SD Booting Xen and Dom0 | RootFS in Kernel (initramfs), not loading rootfs.cpio.gz.u-boot, boot-up gets further but ends with a kernel panic because the RootFS is indeed missing:

 

   ...

   Loading Kernel Image ... OK

   Loading Device Tree to 0000000007fef000, end 0000000007fff5e8 ... OK

 

Starting kernel ...

 

Xen 4.11.1-pre

(XEN) Xen version 4.11.1-pre (@) (aarch64-xilinx-linux-gcc (GCC) 7.3.0) debug=n  Mon Dec  3 21:50:14 UTC 2018

(XEN) Latest ChangeSet: Thu Nov 8 15:40:11 2018 -0800 git:b2edf52-dirty

(XEN) Processor: 410fd034: "ARM Limited", variant: 0x0, part 0xd03, rev 0x4

(XEN) 64-bit Execution:

(XEN)   Processor Features: 0000000000002222 0000000000000000

(XEN)     Exception Levels: EL3:64+32 EL2:64+32 EL1:64+32 EL0:64+32

(XEN)     Extensions: FloatingPoint AdvancedSIMD

(XEN)   Debug Features: 0000000010305106 0000000000000000

(XEN)   Auxiliary Features: 0000000000000000 0000000000000000

(XEN)   Memory Model Features: 0000000000001122 0000000000000000

(XEN)   ISA Features:  0000000000011120 0000000000000000

(XEN) 32-bit Execution:

(XEN)   Processor Features: 00000131:00011011

(XEN)     Instruction Sets: AArch32 A32 Thumb Thumb-2 Jazelle

(XEN)     Extensions: GenericTimer Security

(XEN)   Debug Features: 03010066

(XEN)   Auxiliary Features: 00000000

(XEN)   Memory Model Features: 10201105 40000000 01260000 02102211

(XEN)  ISA Features: 02101110 13112111 21232042 01112131 00011142 00011121

(XEN) Generic Timer IRQ: phys=30 hyp=26 virt=27 Freq: 100000 KHz

(XEN) GICv2 initialization:

(XEN)         gic_dist_addr=00000000f9010000

(XEN)         gic_cpu_addr=00000000f9020000

(XEN)         gic_hyp_addr=00000000f9040000

(XEN)         gic_vcpu_addr=00000000f9060000

(XEN)         gic_maintenance_irq=25

(XEN) GICv2: Adjusting CPU interface base to 0xf902f000

(XEN) GICv2: 192 lines, 4 cpus, secure (IID 0200143b).

(XEN) Using scheduler: SMP Credit Scheduler (credit)

(XEN) Allocated console ring of 16 KiB.

(XEN) Bringing up CPU1

(XEN) Bringing up CPU2

(XEN) Bringing up CPU3

(XEN) Brought up 4 CPUs

(XEN) P2M: 40-bit IPA with 40-bit PA and 8-bit VMID

(XEN) P2M: 3 levels with order-1 root, VTCR 0x80023558

(XEN) I/O virtualisation enabled

(XEN)  - Dom0 mode: Relaxed

(XEN) Interrupt remapping enabled

(XEN) *** LOADING DOMAIN 0 ***

(XEN) Loading kernel from boot module @ 0000000000080000

(XEN) Allocating 1:1 mappings totalling 768MB for dom0:

(XEN) BANK[0] 0x00000020000000-0x00000040000000 (512MB)

(XEN) BANK[1] 0x00000060000000-0x00000070000000 (256MB)

(XEN) Grant table range: 0x0000007fc00000-0x0000007fc40000

(XEN) Allocating PPI 16 for event channel interrupt

(XEN) Loading zImage from 0000000000080000 to 0000000020080000-0000000023180000

(XEN) Loading dom0 DTB to 0x0000000028000000-0x000000002800be15

(XEN) Initial low memory virq threshold set at 0x4000 pages.

(XEN) Std. Loglevel: Errors and warnings

(XEN) Guest Loglevel: Nothing (Rate-limited: Errors and warnings)

(XEN) *** Serial input -> DOM0 (type 'CTRL-a' three times to switch input to Xen)

(XEN) Freed 280kB init memory.

(XEN) d0v0: vGICD: unhandled word write 0xffffffff to ICACTIVER4

(XEN) d0v0: vGICD: unhandled word write 0xffffffff to ICACTIVER8

(XEN) d0v0: vGICD: unhandled word write 0xffffffff to ICACTIVER12

(XEN) d0v0: vGICD: unhandled word write 0xffffffff to ICACTIVER16

(XEN) d0v0: vGICD: unhandled word write 0xffffffff to ICACTIVER20

(XEN) d0v0: vGICD: unhandled word write 0xffffffff to ICACTIVER0

[    0.000000] Booting Linux on physical CPU 0x0

[    0.000000] Linux version 4.14.0-xilinx-v2018.3 (oe-user@oe-host) (gcc version 7.3.0 (GCC)) #1 SMP Fri Oct 4 11:17:48 UTC 2019

[    0.000000] Boot CPU: AArch64 Processor [410fd034]

[    0.000000] Machine model: Avnet Ultra96 Rev1

...

[    4.595713]   b301         1048576 mmcblk0p1 3cd596cb-01

[    4.595715]

[    4.602629]   b302        30116864 mmcblk0p2 3cd596cb-02

[    4.602631]

[    4.609555] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

[    4.617858] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.14.0-xilinx-v2018.3 #1

[    4.625116] Hardware name: Avnet Ultra96 Rev1 (DT)

[    4.629961] Call trace:

[    4.632483] [<ffffff8008088c58>] dump_backtrace+0x0/0x368

[    4.637925] [<ffffff8008088fd4>] show_stack+0x14/0x20

[    4.643027] [<ffffff8008a4d9f8>] dump_stack+0x9c/0xbc

[    4.648133] [<ffffff800809bdc0>] panic+0x11c/0x274

[    4.652975] [<ffffff8008db1124>] mount_block_root+0x1a8/0x27c

[    4.658767] [<ffffff8008db1430>] mount_root+0x11c/0x134

[    4.664043] [<ffffff8008db15b4>] prepare_namespace+0x16c/0x1b4

[    4.669925] [<ffffff8008db0d44>] kernel_init_freeable+0x1b8/0x1d8

[    4.676069] [<ffffff8008a5fd48>] kernel_init+0x10/0x100

[    4.681344] [<ffffff8008084a90>] ret_from_fork+0x10/0x18

[    4.686709] Kernel Offset: disabled

[    4.690255] CPU features: 0x002004

[    4.693711] Memory Limit: none

[    4.696829] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

 

Thanks in advance for any help.

  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi there,

     

    While we do not support Xen, nor the build images, have you checked the Vivado project / HDF?  That is where all the RAM locations are defined.

    As this is so related to Xen and Xilinx instructions / designs, you might have better luck with this question over at the Xilinx forum.

     

    --Dan