Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Booting Ultra96-V2 From OOB Image
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 365 subscribers
  • Views 2501 views
  • Users 0 members are here
Related

Booting Ultra96-V2 From OOB Image

the_durst
the_durst over 6 years ago

Hello,

 

I'm having trouble following the instructions on page 11 of http://zedboard.org/sites/default/files/documentations/Ultra96-V2-GSG-v1_1.pdf for section 6 Example Design. I've installed the image on a microSD card using balenaEtcher (following the advice of https://www.96boards.org/documentation/consumer/ultra96/ultra96-v2/getting-started/ ), but the Ultra96V2 boot seems to stall. As you can see from the logs emitted over the UART/JTAG serial connection below, the boot stalls before it gets to the login section. Also, I've verified that no wireless network is being created. Finally, I see no output on a monitor when I boot with a mouse, keyboard, and displayport monitor plugged in.

 

This used to work a couple days ago. I used to be able to boot the Ultra96V2 by microSD card, log in via the UART/JTAG connection, and connect to the Ultra96V2's wifi network. However, since creating that working microSD card image, I've reflashed the microSD card with a couple of other apps created by following | Zedboard. Now, when I reflash the microSDcard with the OOB image, the boot stalls as explained above and shown below.

 

I reflashed the microSD card with other apps including Vitis's hello world and mem test applications. The hello world one works from the microSD card, but the mem test stalls after the FSBL runs. I've verified that both of those apps run correctly when run on the Ultra96V2 by UART/JTAG.

 

=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2020.06.07 11:33:15 =~=~=~=~=~=~=~=~=~=~=~=
Xilinx Zynq MP First Stage Boot Loader 

Release 2018.3   Aug 28 2019  -  15:56:54
PMUFW:    v1.1


U-Boot 2018.01 (Aug 28 2019 - 15:55:40 +0000)

Model: Avnet Ultra96 Rev1
Board: Xilinx ZynqMP
I2C:   ready
DRAM:  2 GiB
EL Level:    EL2
Chip ID:    zu3eg
Watchdog: Started
MMC:   mmc@ff160000: 0 (SD), mmc@ff170000: 1
*** Warning - bad CRC, using default environment

In:    serial@ff010000
Out:   serial@ff010000
Err:   serial@ff010000
Model: Avnet Ultra96 Rev1
Board: Xilinx ZynqMP
Bootmode: SD_MODE
Net:   Net Initialization Skipped
No ethernet found.
U-BOOT for ultra96v2-oob-2018-3

Hit any key to stop autoboot:  2     1     0 
Device: mmc@ff160000
Manufacturer ID: 58
OEM: 4444
Name: DDINC 
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.9 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading image.ub
7183288 bytes read in 523 ms (13.1 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
   Using 'conf@system-top.dtb' configuration
   Trying 'kernel@1' kernel subimage
     Description:  Linux kernel
     Type:         Kernel Image
     Compression:  gzip compressed
     Data Start:   0x10000108
     Data Size:    7127998 Bytes = 6.8 MiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x00080000
     Entry Point:  0x00080000
     Hash algo:    sha1
     Hash value:   04f9659080d961d4edffa5b263d7a59134ceff7a
   Verifying Hash Integrity ... sha1+ OK
## Loading fdt from FIT Image at 10000000 ...
   Using 'conf@system-top.dtb' configuration
   Trying 'fdt@system-top.dtb' fdt subimage
     Description:  Flattened Device Tree blob
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0x106cc5cc
     Data Size:    53366 Bytes = 52.1 KiB
     Architecture: AArch64
     Hash algo:    sha1
     Hash value:   4120cc155aa00b15cf5b2b96925266a26a90001e
   Verifying Hash Integrity ... sha1+ OK
   Booting using the fdt blob at 0x106cc5cc
   Uncompressing Kernel Image ... OK
   Loading Device Tree to 0000000007fef000, end 0000000007fff075 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.14.0-xilinx-v2018.3 (oe-user@oe-host) (gcc version 7.3.0 (GCC)) #1 SMP Wed Aug 28 15:59:03 UTC 2019
[    0.000000] Boot CPU: AArch64 Processor [410fd034]
[    0.000000] Machine model: Avnet Ultra96 Rev1
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8')
[    0.000000] bootconsole [cdns0] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 256 MiB at 0x000000006fc00000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] random: fast init done
[    0.000000] percpu: Embedded 21 pages/cpu @ffffffc07fe60000 s46488 r8192 d31336 u86016
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 512771
[    0.000000] Kernel command line: earlycon console=ttyPS0,115200 clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait
[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)
[    0.000000] Memory: 1768068K/2079744K available (10172K kernel code, 666K rwdata, 3256K rodata, 512K init, 2360K bss, 49532K reserved, 262144K cma-reserved)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)
[    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)
[    0.000000]       .text : 0xffffff8008080000 - 0xffffff8008a70000   ( 10176 KB)
[    0.000000]     .rodata : 0xffffff8008a70000 - 0xffffff8008db0000   (  3328 KB)
[    0.000000]       .init : 0xffffff8008db0000 - 0xffffff8008e30000   (   512 KB)
[    0.000000]       .data : 0xffffff8008e30000 - 0xffffff8008ed6a00   (   667 KB)
[    0.000000]        .bss : 0xffffff8008ed6a00 - 0xffffff8009124db0   (  2361 KB)
[    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)
[    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)
[    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)
[    0.000000]               0xffffffbf00000000 - 0xffffffbf01bfc800   (    27 MB actual)
[    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc07ff00000   (  2047 MB)
[    0.000000] Hierarchical RCU implementation.
[    0.000000]     RCU event tracing is enabled.
[    0.000000]     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
[    0.000004] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
[    0.008440] Console: colour dummy device 80x25
[    0.012481] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000)
[    0.022840] pid_max: default: 32768 minimum: 301
[    0.027538] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes)
[    0.034095] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)
[    0.041952] ASID allocator initialised with 65536 entries
[    0.046596] Hierarchical SRCU implementation.
[    0.051215] EFI services will not be available.
[    0.055387] zynqmp_plat_init Platform Management API v1.1
[    0.060729] zynqmp_plat_init Trustzone version v1.0
[    0.065677] smp: Bringing up secondary CPUs ...
[    0.207016] Detected VIPT I-cache on CPU1
[    0.207058] CPU1: Booted secondary processor [410fd034]
[    0.319170] Detected VIPT I-cache on CPU2
[    0.319189] CPU2: Booted secondary processor [410fd034]
[    0.444927] Detected VIPT I-cache on CPU3
[    0.444946] CPU3: Booted secondary processor [410fd034]
[    0.444990] smp: Brought up 1 node, 4 CPUs
[    0.470952] SMP: Total of 4 processors activated.
[    0.475626] CPU features: detected feature: 32-bit EL0 Support
[    0.481424] CPU: All CPU(s) started at EL2
[    0.485496] alternatives: patching kernel code
[    0.490632] devtmpfs: initialized
[    0.498886] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.502980] futex hash table entries: 1024 (order: 5, 131072 bytes)
[    0.515606] xor: measuring software checksum speed
[    0.553306]    8regs     :  2303.000 MB/sec
[    0.593334]    8regs_prefetch:  2053.000 MB/sec
[    0.633362]    32regs    :  2830.000 MB/sec
[    0.673392]    32regs_prefetch:  2379.000 MB/sec
[    0.673424] xor: using function: 32regs (2830.000 MB/sec)
[    0.677825] pinctrl core: initialized pinctrl subsystem
[    0.683617] NET: Registered protocol family 16
[    0.688076] cpuidle: using governor menu
[    0.691831] vdso: 2 pages (1 code @ ffffff8008a76000, 1 data @ ffffff8008e34000)
[    0.698587] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.705933] DMA: preallocated 256 KiB pool for atomic allocations
[    0.732914] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed
[    0.734901] ARM CCI_400_r1 PMU driver probed
[    0.739559] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized
[    0.755736] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.823236] raid6: int64x1  gen()   402 MB/s
[    0.891175] raid6: int64x1  xor()   444 MB/s
[    0.959225] raid6: int64x2  gen()   689 MB/s
[    1.027287] raid6: int64x2  xor()   602 MB/s
[    1.095329] raid6: int64x4  gen()  1042 MB/s
[    1.163353] raid6: int64x4  xor()   741 MB/s
[    1.231457] raid6: int64x8  gen()   980 MB/s
[    1.299473] raid6: int64x8  xor()   745 MB/s
[    1.367493] raid6: neonx1   gen()   726 MB/s
[    1.435547] raid6: neonx1   xor()   853 MB/s
[    1.503632] raid6: neonx2   gen()  1170 MB/s
[    1.571634] raid6: neonx2   xor()  1207 MB/s
[    1.639692] raid6: neonx4   gen()  1504 MB/s
[    1.707735] raid6: neonx4   xor()  1441 MB/s
[    1.775806] raid6: neonx8   gen()  1652 MB/s
[    1.843826] raid6: neonx8   xor()  1532 MB/s
[    1.843855] raid6: using algorithm neonx8 gen() 1652 MB/s
[    1.847815] raid6: .... xor() 1532 MB/s, rmw enabled
[    1.852746] raid6: using neon recovery algorithm
[    1.858068] XGpio: /amba_pl@0/gpio@a0020000: registered, base is 511
[    1.863775] PLL: shutdown
[    1.866248] zynqmp_pll_disable() clock disable failed for iopll_int, ret = -13
[    1.873618] XGpio: /amba_pl@0/gpio@a0020000: dual channel registered, base is 510
[    1.881211] XGpio: /amba_pl@0/gpio@a0021000: registered, base is 509
[    1.887416] XGpio: /amba_pl@0/gpio@a0022000: registered, base is 507
[    1.893618] PLL: shutdown
[    1.896186] XGpio: /amba_pl@0/gpio@a0022000: dual channel registered, base is 505
[    1.904781] SCSI subsystem initialized
[    1.907448] usbcore: registered new interface driver usbfs
[    1.912730] usbcore: registered new interface driver hub
[    1.918012] usbcore: registered new device driver usb
[    1.923051] media: Linux media interface: v0.10
[    1.927505] Linux video capture interface: v2.00
[    1.932105] pps_core: LinuxPPS API ver. 1 registered
[    1.936998] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    1.946091] PTP clock support registered
[    1.949991] EDAC MC: Ver: 3.0.0
[    1.953239] PLL: shutdown
[    1.955941] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.
[    1.962713] FPGA manager framework
[    1.966005] fpga-region fpga-full: FPGA Region probed
[    1.971021] Advanced Linux Sound Architecture Driver Initialized.
[    1.977275] Bluetooth: Core ver 2.22
[    1.980522] NET: Registered protocol family 31
[    1.984920] Bluetooth: HCI device and connection manager initialized
[    1.991237] Bluetooth: HCI socket layer initialized
[    1.996079] Bluetooth: L2CAP socket layer initialized
[    2.001113] Bluetooth: SCO socket layer initialized
[    2.006608] clocksource: Switched to clocksource arch_sys_counter
[    2.012087] VFS: Disk quotas dquot_6.6.0
[    2.015934] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    2.027040] NET: Registered protocol family 2
[    2.027439] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[    2.034331] TCP bind hash table entries: 16384 (order: 6, 262144 bytes)
[    2.041148] TCP: Hash tables configured (established 16384 bind 16384)
[    2.047392] UDP hash table entries: 1024 (order: 3, 32768 bytes)
[    2.053290] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
[    2.059793] NET: Registered protocol family 1
[    2.064225] RPC: Registered named UNIX socket transport module.
[    2.069867] RPC: Registered udp transport module.
[    2.074533] RPC: Registered tcp transport module.
[    2.079204] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    2.086229] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    2.092875] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    2.101281] audit: initializing netlink subsys (disabled)
[    2.105841] audit: type=2000 audit(2.056:1): state=initialized audit_enabled=0 res=1
[    2.106198] workingset: timestamp_bits=62 max_order=19 bucket_order=0
[    2.120639] NFS: Registering the id_resolver key type
[    2.124900] Key type id_resolver registered
[    2.129029] Key type id_legacy registered
[    2.133014] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    2.139682] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    2.169371] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[    2.171127] io scheduler noop registered
[    2.175013] io scheduler deadline registered
[    2.179262] io scheduler cfq registered (default)
[    2.183922] io scheduler mq-deadline registered
[    2.188419] io scheduler kyber registered
[    2.194046] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[    2.199155] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
[    2.205787] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
[    2.212709] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
[    2.219626] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
[    2.226549] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
[    2.233466] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
[    2.240384] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
[    2.247305] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
[    2.254298] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success
[    2.261148] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success
[    2.268063] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success
[    2.274982] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success
[    2.281901] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success
[    2.288824] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success
[    2.295747] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success
[    2.302673] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success
[    2.342469] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    2.345084] a0000000.serial: ttyS3 at MMIO 0xa0001000 (irq = 50, base_baud = 6250000) is a 16550A
[    2.352654] a0010000.serial: ttyS1 at MMIO 0xa0011000 (irq = 51, base_baud = 6250000) is a 16550A
[    2.363744] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    2.371737] brd: module loaded
[    2.375896] loop: module loaded
[    2.376966] mtdoops: mtd device (mtddev=name/number) must be supplied
[    2.381992] libphy: Fixed MDIO Bus: probed
[    2.385027] tun: Universal TUN/TAP device driver, 1.6
[    2.389110] CAN device driver interface
[    2.393793] usbcore: registered new interface driver asix
[    2.398132] usbcore: registered new interface driver ax88179_178a
[    2.404140] usbcore: registered new interface driver cdc_ether
[    2.409935] usbcore: registered new interface driver net1080
[    2.415556] usbcore: registered new interface driver cdc_subset
[    2.421439] usbcore: registered new interface driver zaurus
[    2.426988] usbcore: registered new interface driver cdc_ncm
[    2.432986] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    2.439359] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    2.445303] ehci-pci: EHCI PCI platform driver
[    2.450043] usbcore: registered new interface driver uas
[    2.455016] usbcore: registered new interface driver usb-storage
[    2.461590] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
[    2.468190] i2c /dev entries driver
[    2.472582] IR NEC protocol handler initialized
[    2.476085] IR RC5(x/sz) protocol handler initialized
[    2.481100] IR RC6 protocol handler initialized
[    2.485597] IR JVC protocol handler initialized
[    2.490096] IR Sony protocol handler initialized
[    2.494679] IR SANYO protocol handler initialized
[    2.499351] IR Sharp protocol handler initialized
[    2.504022] IR MCE Keyboard/mouse protocol handler initialized
[    2.509817] IR XMP protocol handler initialized
[    2.515915] usbcore: registered new interface driver uvcvideo
[    2.520026] USB Video Class driver (1.1.1)
[    2.525090] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff80091d5000 with timeout 60s
[    2.533409] cdns-wdt ff150000.watchdog: Xilinx Watchdog Timer at ffffff80091dd000 with timeout 10s
[    2.542155] Bluetooth: HCI UART driver ver 2.3
[    2.546329] Bluetooth: HCI UART protocol H4 registered
[    2.551425] Bluetooth: HCI UART protocol BCSP registered
[    2.556725] Bluetooth: HCI UART protocol LL registered
[    2.561805] Bluetooth: HCI UART protocol ATH3K registered
[    2.567167] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    2.573442] Bluetooth: HCI UART protocol Intel registered
[    2.578759] Bluetooth: HCI UART protocol QCA registered
[    2.583984] usbcore: registered new interface driver bcm203x
[    2.589600] usbcore: registered new interface driver bpa10x
[    2.595138] usbcore: registered new interface driver bfusb
[    2.600584] usbcore: registered new interface driver btusb
[    2.606007] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[    2.611675] usbcore: registered new interface driver ath3k
[    2.617217] EDAC MC: ECC not enabled
[    2.620859] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[    2.633875] sdhci: Secure Digital Host Controller Interface driver
[    2.638877] sdhci: Copyright(c) Pierre Ossman
[    2.643201] sdhci-pltfm: SDHCI platform and OF driver helper
[    2.694619] mmc0: SDHCI controller on ff160000.mmc [ff160000.mmc] using ADMA 64-bit
[    2.702948] ledtrig-cpu: registered to indicate activity on CPUs
[    2.703493] usbcore: registered new interface driver usbhid
[    2.708848] usbhid: USB HID core driver
[    2.714778] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    2.719479] usbcore: registered new interface driver snd-usb-audio
[    2.726118] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    2.831200] Netfilter messages via NETLINK v0.30.
[    2.831373] ip_tables: (C) 2000-2006 Netfilter Core Team
[    2.836725] Initializing XFRM netlink socket
[    2.839858] NET: Registered protocol family 10
[    2.846655] Segment Routing with IPv6
[    2.847866] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    2.853328] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    2.859458] NET: Registered protocol family 17
[    2.863495] NET: Registered protocol family 15
[    2.867912] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    2.880784] Ebtables v2.0 registered
[    2.884451] can: controller area network core (rev 20170425 abi 9)
[    2.890555] NET: Registered protocol family 29
[    2.894893] can: raw protocol (rev 20170425)
[    2.899123] can: broadcast manager protocol (rev 20170425 t)
[    2.904748] can: netlink gateway (rev 20170425) max_hops=1
[    2.910303] Bluetooth: RFCOMM TTY layer initialized
[    2.915045] Bluetooth: RFCOMM socket layer initialized
[    2.920156] Bluetooth: RFCOMM ver 1.11
[    2.923864] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    2.929136] Bluetooth: BNEP filters: protocol multicast
[    2.934329] Bluetooth: BNEP socket layer initialized
[    2.939260] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    2.945142] Bluetooth: HIDP socket layer initialized
[    2.950235] 9pnet: Installing 9P2000 support
[    2.954329] Key type dns_resolver registered
[    2.959084] registered taskstats version 1
[    2.963051] Btrfs loaded, crc32c=crc32c-generic
[    2.972830] ff000000.serial: ttyPS2 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps
[    2.976771] ff010000.serial: ttyPS0 at MMIO 0xff010000 (irq = 41, base_baud = 6249999) is a xuartps
·          ’&)Ê‚ººÊê  ½¹Í½±•ÚÑÑåAMÁê*¹…‰±•‘5RÚ    ’rÊÊ‚ººÊê  ½¹Í½±•ÚÑÑåAMÁê*¹…‰±•‘5RÚ    ’rÊÊ¢š²šê  ½½Ñ½¹Í½±•Ú‘¹ÍÁê"¥Í…‰±•‘5RÚ    ’rÊÊ¢š²šê  ½½Ñ½¹Í½±•Ú‘¹ÍÁê"¥Í…‰±•‘5RÚ    šr‚‚ššš²ê Â¥±¥¹áµ‚͝ÑɁ2‘Ñ‚‚‚‚‚rÒå¹ÅµÁ}Á¡åé b ¹•éŠ ¢åÁ•é ‚ɽѽ½±é¢ ‚±±}±½•‘éÊ•Í5Rþ[    3.013984] PLL: shutdown
[    3.016700] PLL: shutdown
[    3.019821] PLL: enable
[    3.022356] PLL: shutdown
[    3.026033] PLL: enable
[    3.028564] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
[    3.039159] mmc0: new high speed SDHC card at address 5048
[    3.039292] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[    3.039516] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[    3.040150] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.040259] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.085204] mmcblk0: mmc0:5048 DDINC 14.9 GiB 
[    3.111359]  mmcblk0: p1 p2
[    3.174711] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
[    3.184933] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[    3.191973] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    3.198580] [drm] No driver support for vblank timestamp query.
[    3.204573] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008b28168)
[    4.290622] [drm] Cannot find any crtc or sizes
[    4.347018] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
[    4.355124] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
[    4.364958] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
[    4.376447] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:1 protocol:3 pll_locked:yes
[    4.386497] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    4.391995] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    4.399872] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010
[    4.408607] xhci-hcd xhci-hcd.0.auto: irq 61, io mem 0xfe300000
[    4.414670] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    4.421454] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    4.428665] usb usb1: Product: xHCI Host Controller
[    4.433534] usb usb1: Manufacturer: Linux 4.14.0-xilinx-v2018.3 xhci-hcd
[    4.440226] usb usb1: SerialNumber: xhci-hcd.0.auto
[    4.445527] hub 1-0:1.0: USB hub found
[    4.449296] hub 1-0:1.0: 1 port detected
[    4.453404] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    4.458890] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[    4.466621] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    4.474778] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[    4.481565] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    4.488775] usb usb2: Product: xHCI Host Controller
[    4.493645] usb usb2: Manufacturer: Linux 4.14.0-xilinx-v2018.3 xhci-hcd
[    4.500337] usb usb2: SerialNumber: xhci-hcd.0.auto
[    4.505452] hub 2-0:1.0: USB hub found
[    4.509214] hub 2-0:1.0: 1 port detected
[    4.514928] i2c i2c-0: Added multiplexed i2c bus 2
[    4.519865] i2c i2c-0: Added multiplexed i2c bus 3
[    4.524795] i2c i2c-0: Added multiplexed i2c bus 4
[    4.529730] i2c i2c-0: Added multiplexed i2c bus 5
[    4.535248] tps65086 6-005e: Failed to read revision register
[    4.541100] i2c i2c-0: Added multiplexed i2c bus 6
[    4.546496] ina2xx 7-0040: error configuring the device: -6
[    4.552115] i2c i2c-0: Added multiplexed i2c bus 7
[    4.557085] i2c i2c-0: Added multiplexed i2c bus 8
[    4.562016] i2c i2c-0: Added multiplexed i2c bus 9
[    4.566804] pca954x 0-0075: registered 8 multiplexed busses for I2C switch pca9548
[    4.574414] i2c i2c-0: Failed to register i2c client pca9548 at 0x75 (-16)
[    4.581280] i2c i2c-0: of_i2c: Failure registering /amba/i2c@ff030000/i2cswitch@75
[    4.588840] i2c i2c-0: Failed to create I2C device for /amba/i2c@ff030000/i2cswitch@75
[    4.596749] cdns-i2c ff030000.i2c: 100 kHz mmio ff030000 irq 31
[    4.604428] sdhci-arasan ff170000.mmc: allocated mmc-pwrseq
[    4.654618] mmc1: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
[    4.669788] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[    4.676763] rtc_zynqmp ffa60000.rtc: setting system clock to 1970-01-01 00:00:06 UTC (6)
[    4.684902] of_cfs_init
[    4.687365] of_cfs_init: OK
[    4.690308] clk: Not disabling unused clocks
[    4.694797] ALSA device list:
[    4.697747]   #0: DisplayPort monitor
[    4.705136] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
[    4.716397] mmc1: new high speed SDIO card at address 0001
[    4.790622] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[    4.943094] usb 1-1: New USB device found, idVendor=0424, idProduct=2744
[    4.949798] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    4.956928] usb 1-1: Product: USB2744
[    4.960586] usb 1-1: Manufacturer: Microchip Tech
[    5.042693] hub 1-1:1.0: USB hub found
[    5.046462] hub 1-1:1.0: 4 ports detected
[    5.074567] usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd
[    5.098986] usb 2-1: New USB device found, idVendor=0424, idProduct=5744
[    5.105685] usb 2-1: New USB device strings: Mfr=2, Product=3, SerialNumber=0
[    5.112817] usb 2-1: Product: USB5744
[    5.116469] usb 2-1: Manufacturer: Microchip Tech
[    5.122674] hub 2-1:1.0: USB hub found
[    5.126461] hub 2-1:1.0: 3 ports detected
[    5.313031] EXT4-fs (mmcblk0p2): recovery complete
[    5.317826] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    5.325937] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    5.366615] usb 1-1.4: new high-speed USB device number 3 using xhci-hcd
[    5.395993] devtmpfs: mounted
[    5.398621] [drm] Cannot find any crtc or sizes
[    5.403702] Freeing unused kernel memory: 512K
[    5.471288] usb 1-1.4: New USB device found, idVendor=0424, idProduct=2740
[    5.478160] usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    5.485458] usb 1-1.4: Product: Hub Controller
[    5.489892] usb 1-1.4: Manufacturer: Microchip Tech
[   16.394607] mmc0: Timeout waiting for hardware interrupt.
[   16.400000] mmc0: sdhci: ============ SDHCI REGISTER DUMP ===========
[   16.406423] mmc0: sdhci: Sys addr:  0x000000a0 | Version:  0x00001002
[   16.412846] mmc0: sdhci: Blk size:  0x00007200 | Blk cnt:  0x00000000
[   16.419269] mmc0: sdhci: Argument:  0x00602808 | Trn mode: 0x0000003b
[   16.425692] mmc0: sdhci: Present:   0x01f70000 | Host ctl: 0x0000001f
[   16.432115] mmc0: sdhci: Power:     0x0000000f | Blk gap:  0x00000080
[   16.438539] mmc0: sdhci: Wake-up:   0x00000000 | Clock:    0x00000207
[   16.444962] mmc0: sdhci: Timeout:   0x00000004 | Int stat: 0x00000003
[   16.451385] mmc0: sdhci: Int enab:  0x02ff008b | Sig enab: 0x02ff008b
[   16.457808] mmc0: sdhci: AC12 err:  0x00000000 | Slot int: 0x00000001
[   16.464232] mmc0: sdhci: Caps:      0x31e8c881 | Caps_1:   0x00002007
[   16.470655] mmc0: sdhci: Cmd:       0x0000123a | Max curr: 0x00000000
[   16.477078] mmc0: sdhci: Resp[0]:   0x00000900 | Resp[1]:  0x00775f7f
[   16.483501] mmc0: sdhci: Resp[2]:   0x325b5900 | Resp[3]:  0x00000900
[   16.489924] mmc0: sdhci: Host ctl2: 0x00000000
[   16.494351] mmc0: sdhci: ADMA Err:  0x00000000 | ADMA Ptr: 0x000000006fc40230
[   16.501468] mmc0: sdhci: ============================================

 

Thank you for your help!

  • Sign in to reply
  • Cancel

Top Replies

  • the_durst
    the_durst over 6 years ago +1 verified
    I bought a new microSD card ( https://www.amazon.com/gp/product/B0887GP791 ) and it started working. The board now boots to a login screen and I can log in. The one that shipped with the Ultra96v2 must…
Parents
  • narrucmot
    0 narrucmot over 6 years ago

    Are you using the same 16GB SD card that came with the Ultra96-V2 board?  If not, are you using a 8GB SD card?  Even though the provided OOB OS image is also 8GB, not all SD cards are created equally.  Even though marked as 8GB, their actual capacities may be different.  We have seen cases where the OS image is written to a 8GB SD card and the boot will fail in strange ways, often like you describe.  This is because the imaging software (Etcher or Win32DiskImager) does not correctly detect that the OS image size is larger than the actual capacity of the SD card.  The result is the OS image will be written to the SD card, but strange behavior and boot failures will occur.  That is why we recommend using the provided 16GB SD card when imaging the OS to the SD card.  This will result in (nearly) 8GB of the SD card being unused, but it is known to always work.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • the_durst
    0 the_durst over 6 years ago in reply to narrucmot

    Hi Tom,

     

    Thank you for your help!

     

    I am using the 16 GB Delkin Devices microSD card that came with the Ultra96-V2 board. Booting with this card produced the previously supplied errors.

     

    I've also tried another 16 GB microSD card (https://www.amazon.com/gp/product/B07RPVH4QQ ) and I'm seeing similar errors.

     

    Please let me know if you have other advice. Thank you again!

     

    Thanks,

    David Durst

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • the_durst
    0 the_durst over 6 years ago in reply to narrucmot

    Hi Tom,

     

    Thank you for your help!

     

    I am using the 16 GB Delkin Devices microSD card that came with the Ultra96-V2 board. Booting with this card produced the previously supplied errors.

     

    I've also tried another 16 GB microSD card (https://www.amazon.com/gp/product/B07RPVH4QQ ) and I'm seeing similar errors.

     

    Please let me know if you have other advice. Thank you again!

     

    Thanks,

    David Durst