Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design USB and WiFi interfaces
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 365 subscribers
  • Views 976 views
  • Users 0 members are here
Related

USB and WiFi interfaces

talvlad29
talvlad29 over 5 years ago

Hello,

I use 2019.2 Vivado, Vitis and Petalinux versions to build my design and Linux configuration. My design includes USB 3.0 interface and WiFi (wilc driver 15.2). I successfully connect Ultra96v2 board to WiFi and get remote access to the board via SSH (I use OpenSSH) if there is no external USB devices. It works well if I plug USB 3.0 device to J9 USB connector. However, I SSH gets hang if I plug USB device to J8 connector. SSH comes back after unplugging USB device from J8 connector. What can cause this issue?

Thank you,

Vladimir

  • Sign in to reply
  • Cancel

Top Replies

  • narrucmot
    narrucmot over 5 years ago +1 suggested
    Hi Vladimir, This is a known issue with the Ultra96 board. The issue is that the USB 3.0 transceivers, when active (something is plugged into the J8 and/or possibly J9 USB host connectors), emit enough…
  • narrucmot
    0 narrucmot over 5 years ago

    Hi Vladimir,

     

    This is a known issue with the Ultra96 board.  The issue is that the USB 3.0 transceivers, when active (something is plugged into the J8 and/or possibly J9 USB host connectors), emit enough EMI to interfere with the WiFi and cripple its throughput.  This would certainly affect ssh and WiFi traffic.  An alternative, if possible, is to use a USB-to-Ethernet adapter like these:

    USB 3.0 to GbE AdapterUSB 3.0 to GbE Adapter

    https://www.amazon.com/TRENDnet-Ethernet-Chromebook-Specific-TU3-ETG/dp/B00FFJ0RKE/

     

    You could also enable USB gadget Ethernet, but that is a bit more complicated.  I will be posting a blog about how to do that soon.

     

    Hope this helps.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • talvlad29
    0 talvlad29 over 5 years ago in reply to narrucmot

    Hi Tom,

     

    Thank you for your explanation. You suggested to use USB-to-Ethernet adapter but the problem is I need USB 3.0 to receive high speed data stream and I cannot share it with another task.

     

    Thank you,

     

    Vladimir

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 5 years ago in reply to talvlad29

    A little bit more investigation indicates that USB 3.0 interference with WiFi is a known issue for all kinds of products.  This is because the noise coming off an active USB 3.0 port is in the 2.4 GHz range, which is where WiFi operates.  This article describes this issue further:

    https://www.pcmag.com/opinions/wireless-witch-the-truth-about-usb-30-and-wi-fi-interference

     

    So this is something that is definitely not unique to the Ultra96 board, though it may be exacerbated by the fact that the USB 3.0 connectors (noise radiators) are so close to the WiFi module and antenna.  Hopefully your workaround of plugging your USB 3.0 device into J8 instead of J9 is acceptable.  Maybe a USB cable with better shielding will also help?

     

    --Tom