Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96-V2 - Engineering & Technology - Documentation
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 365 subscribers
  • Views 1255 views
  • Users 0 members are here
Related

Ultra96-V2 - Engineering & Technology - Documentation

jomoenginer
jomoenginer over 5 years ago

From the Ultra96-V2 page under Reference Designs there are links to a 'sharepoint' for items such as:

https://www.element14.com/community/docs/DOC-95649/l/ultra96-v2

 

PetaLinux Board Support Packages

Ultra96-V2 – PetaLinux 2020+ BSP (Sharepoint site)

 

Vitis PetaLinux Platform PreBuilt Example

Ultra96-V2 – Vitis PetaLinux Platform 2020+ Vector Add (Sharepoint site)

 

Which go to the following link:

https://avtinc.sharepoint.com/teams/ET-Downloads/Shared%20Documents/Forms/AllItems.aspx?originalPath=aHR0cHM6Ly9hdnRpbmMuc2hhcmVwb2ludC5jb20vOmY6L3QvRVQtRG93bmxvYWRzL0VpYUJ6ZkRrRHI5Sm8yT1FONTJ6b1FzQkQxUkdEcUJIdDVtYTEwSjFzVWloVXc%5FcnRpbWU9Z0pzQ25Dcm4yRWc&viewid=dba68156%2Dce4b%2D4ebb%2Db7a7%2Dec03b27b013d&id=%2Fteams%2FET%2DDownloads%2FShared%20Documents%2Fprojects%2Fpublic%5Frelease%2F2020%2E1

 

Under the '202.2' folder, the only thing listed is the VM Install doc yet the other 2 folders, 2019.2 and 2020.1 list: Vitis_PreBuilt_Example, BSP, OOB, Vitis_Platform, Vitis_PreBuilt_Example.

 

Are these examples available for Vitis and PetaLinux 2020.2?

  • Sign in to reply
  • Cancel

Top Replies

  • narrucmot
    narrucmot over 5 years ago +1 suggested
    Hi Jon, The 2020.2 BSPs, Vitis platforms, etc. for the Ultra96-V2 SBC and UltraZed SOMs, etc. are still in development. We are working on some changes to the rootfs configurations and that is taking longer…
Parents
  • narrucmot
    0 narrucmot over 5 years ago

    Hi Jon,

     

    The 2020.2 BSPs, Vitis platforms, etc. for the Ultra96-V2 SBC and UltraZed SOMs, etc. are still in development.  We are working on some changes to the rootfs configurations and that is taking longer than expected to work through.  We will be making an annouoncement when these BSPs, etc. are released.  Stay tuned!

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 5 years ago

    Hi Jon,

     

    The 2020.2 BSPs, Vitis platforms, etc. for the Ultra96-V2 SBC and UltraZed SOMs, etc. are still in development.  We are working on some changes to the rootfs configurations and that is taking longer than expected to work through.  We will be making an annouoncement when these BSPs, etc. are released.  Stay tuned!

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jomoenginer
    0 jomoenginer over 5 years ago in reply to narrucmot

    Tom,

     

    Okay. Fair enough.

     

    For an Ubuntu install. The 2020.1 version of the Xilinx software is only supported on Ubuntu 18.04.4, or some other earlier versions, but the version listed on the Ubuntu site is 18.04.5 which I had already created a VM from and installed Vitis 2020.2. Trying to install 2020.1 on Ubuntu 18.04.5 results in an unsupported OS warning and then fails with a Java error. I did find some workarounds that were more associated with Red Hat 7.x, but opted to create a new 18.04.4, which is listed as an old release, VM and install 2020.1. After the 2020.1 install, the Xilinx installer prompted to upgrade to 2020.2 which I did not do and then to update 2020.1 to 2020.1.1 which I again did not do.

     

    For the RoadTest I am working on, I'll just stick with the 2020.1 version for now, but see if I can migrate anything up to 2020.2

     

    Thanks,

     

    Jon