Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design High Temperature normal ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 365 subscribers
  • Views 1120 views
  • Users 0 members are here
  • ultra96
Related

High Temperature normal ?

joachimschaefer
joachimschaefer over 5 years ago

Hi, i have a small application with one a53

running, luts 17%


 

but the device was very hot. I have measured 60 *C . This is now within the spec but i would know if this is normal.

 

i am thinking to add a fan to the passive heatsink.



Greetings Joachim

  • Sign in to reply
  • Cancel

Top Replies

  • ctammann
    ctammann over 5 years ago +2 suggested
    Hey Joachim, Couple of questions for you, do you know roughly how much power this design draws? Could you run a vivado power report? Also, where are you reading that temperature? is that reported from…
  • bhfletcher
    bhfletcher over 5 years ago in reply to ctammann +2 suggested
    Another question that I had is whether this is with the new or old heatsink. The new heatsink is really efficient at drawing heat away from the devices on board, meaning you will feel the heat in the heatsink…
  • ctammann
    0 ctammann over 5 years ago

    Hey Joachim,

     

    Couple of questions for you, do you know roughly how much power this design draws? Could you run a vivado power report? Also, where are you reading that temperature? is that reported from the device or using a bench meter? I'm assuming this design is running at room temp. I will say that the Ultra96-V2 can get hot. The heatsink when running our AI design gets very warm, but does not violate the junction temperature requirement. In my testing adding a small fan to the heatsink does drop the PMIC and Xilinx temperature by about 20C.

     

    I guess the main take away is that yes, the device will run hot. At room temperature we can run pretty much anything we want on the board, but know that it will get hot to the touch. Adding a small fan will dramatically drop that temperature, however running a worst case design in my testing showed a max junction temp of about 73C. While that is definitely hot, it does not violate the junction temp requirement.

    Thanks
    Chris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 5 years ago in reply to ctammann

    Another question that I had is whether this is with the new or old heatsink. The new heatsink is really efficient at drawing heat away from the devices on board, meaning you will feel the heat in the heatsink a lot quicker. Even if there is only a small amount of power being drawn, the PMICs are still regulating, and with the internal FETs, they generate heat. Where the old heatsink wasn't in direct thermal contact with the hot parts, a board with the old heatsink may have seemed like it wasn't getting as hot, but the Junction Temp on those parts was actually higher.

     

    Bryan

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer