Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Vitis vs Vivado install
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 365 subscribers
  • Views 4331 views
  • Users 0 members are here
  • ultra96
Related

Vitis vs Vivado install

ChuckMcM
ChuckMcM over 5 years ago

Hi bhfletcher, et al,

 

When I installed Vivado I chose the 'Vivado' option rather than the Vitis option. It seems to have installed a bunch of Vitis components as well but I don't know if it will be ok for doing the courses. Do I uninstall and re-install? Or is there a way to "add" the top level Vitis install to a Vivado install? Or is it all good?

 

I created an RTL project from Vivado and it correctly offered the Ultra96-V2 board  as an option (which I selected) and got to the RTL project window. So from the 'lab/homework' perspective I seem to be Okay but I'm wondering if that is going to be okay for week 3?

 

--Chuck

  • Sign in to reply
  • Cancel

Top Replies

  • ChuckMcM
    ChuckMcM over 5 years ago in reply to narrucmot +3 verified
    Okay, so a bit more context here and so I'm updating this to the correct answer... The answer is start Vivado then select Help->Add Design Tools this will bring up the installer with everything checked…
  • narrucmot
    narrucmot over 5 years ago +2 suggested
    Hi Chuck, You will definitely need to install Vitis. You *should* be able to install Vitis "over the top" of the Vivado you already installed, BUT to be on the safe side I would probably uninstall Vivado…
Parents
  • narrucmot
    0 narrucmot over 5 years ago

    Hi Chuck,

     

    You will definitely need to install Vitis.  You *should* be able to install Vitis "over the top" of the Vivado you already installed, BUT to be on the safe side I would probably uninstall Vivado and then install Vitis (which will also install Vivado).  That will provide the highest degree of certainty that all the tools you need for this webinar series are installed correctly and are ready to use.

     

    --Tom

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ChuckMcM
    0 ChuckMcM over 5 years ago in reply to narrucmot

    Sigh. But understood. Thanks Tom!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ChuckMcM
    0 ChuckMcM over 5 years ago in reply to narrucmot

    Sigh. But understood. Thanks Tom!