Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Board power via USB UART click mezzanine - expected?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 365 subscribers
  • Views 2698 views
  • Users 0 members are here
  • ultra96v2
  • mezzanine
  • usb
  • click
  • power
Related

Board power via USB UART click mezzanine - expected?

dqlb
dqlb over 4 years ago

I have been experimenting with the USB UART click board included with the click mezzanine starter kit (AES-ACC-U96-ME-SK) and was surprised to see that the USB UART/I2C click board appears to be supplying power to the Ultra96 when connected to a powered USB cable, but when the main 12v barrel jack supply is disconnected. It is possible to power on the board with only the click board USB connected (no 12V barrel jack) though the boot does not complete, presumably due to some detection of low power. Furthermore, the VIN_LED, also lights up when ONLY the click board USB cable is connected (no 12v power supply) although noticeably dimmer.

Looking at the Ultra96v2 schematic, this behaviour appears to make some amount of sense, as the 5V output on the low speed expansion header is directly connected to the main 5V rail that feeds into the "Rocky PMICs". However what I cannot explain is why the VIN_LED, which is supposed to indicate that 12V is connected to the board, would light up when only the 5V USB is connected. There doesn't appear to be any direct connection between the 5V rail and the VIN_LED based on the schematic.

The Ultra96 HW user guide does not mention anything about supplying board power with the 5V pin on the low speed expansion header. Is this expected behaviour, or is there potentially something wrong with my board?

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 4 years ago +3
    Here are a few relevant links to various schematics: MIKROE-1985 https://download.mikroe.com/documents/add-on-boards/click/usb-i2c/usb-i2c-click-schematic-v101.pdf 96Boards Click Mezzanine https:/…
  • ctammann
    ctammann over 4 years ago +3
    The short answer is yes, there is a leakage path from output to input on the 38060 (and most switching regulators). As you may know, supporting power from multiple sources becomes a game of "whack a mole…
  • bhfletcher
    bhfletcher over 4 years ago in reply to bhfletcher +2 verified
    My contact at MikroElektronika gave me the following information Some of the early Click boards were developed without a diode. It was intentionally allowed to power up your board with the peripherals…
Parents
  • bhfletcher
    0 bhfletcher over 4 years ago

    Here are a few relevant links to various schematics:

    MIKROE-1985 https://download.mikroe.com/documents/add-on-boards/click/usb-i2c/usb-i2c-click-schematic-v101.pdf

    96Boards Click Mezzanine https://www.avnet.com/opasdata/d120001/medias/docus/197/HW_Click%20Mezzanine_v103_Output%20Files_PDF_Click%20Mezzanine_v103_Schematic.PDF

    Ultra96-V2 /products/devtools/avnetboardscommunity/m/files/1271

    With an active USB cable plugged into MIKROE-1985 while the Ultra96-V2 12V is NOT plugged in:

    • MIKROE-1985 net VCC-5V is active, which enables LDO U2 so VCC-3.3V is also active. Both tie to the Click Site, which connects to the Mezzanine. Both VCC-5V and VCC-3.3V have protection diodes in place preventing backfeed of the USB connector or U2.
    • The Click Mezzanine connects the MIKROE-1985 VCC-5V to VCC_5V, which goes directly to the mezzanine connector and over to the Ultra96-V2. MIKROE-1985 VCC-3.3V connects to mezzanine VCC_3V3, which is also generated from LDO U7 on the mezzanine, but VCC_3V3 does not connect back to Ultra96-V2. Depending on how mezzanine SW1 or SW2 or set, then both VDD and VREF will also be active with either 5V or 3.3V on the mezzanine. This will enable one side of several level shifters as well as the mezzanine ADC U5. However, none of these signals connect back to Ultra96-V2. Therefore, it would appear the VCC_5V on LS connector pin 37 is the culprit.
    • Ultra96-V2 LS Mezzanine (J5) pin 37 connects to net +5.0V. The VIN_LED is D17 and is driven by net +VIN. +VIN does not go very many places
      • +VSYS_IN connects to the LS Mezzanine, but is not connected on the 96Boards Click Mezzanine, so no connection there
      • U19 source voltage for +3V3_PRI, which is not active, so no connection there
      • Possible Fan source voltage through R65, which should be DNP. If R65 and R63 were both populated, you could see the problem, but that would effectively short 5V and 12V which would cause a host of other problems, so I don't think that is it.
      • That leaves Infineon PMIC IR38060 U21. The output is +5.0V while the Vin and PVin inputs are tied to +VIN. This is the only possible connection that I can find, so I am now wondering if there is a feedback path from output to input voltage. I will do some more research with Infineon to find out if this is possible. I will admit that I have definitely seen this with other regulators before in my career, so definitely a possibility.

    The intention was definitely not to supply Ultra96-V2 board power from a Click Site. There is a feature to allow powering the 12V / +VIN through +VSYS_IN on a Mezzanine, but NOT for the 5V or +VCC_PSAUX rails. Perhaps there is more to the Click specification that I'm not familiar with that allows driving 5V back through a Click board. I have asked MikroElektronika for clarification. I do not believe that the MIKROE-1985 should interconnect 5V and 3.3V between the Board and the Mezzanine, but that is what's happening.

    Until we get clarification, I recommend that you do NOT leave the USB cable plugged into the MIKROE-1985 when the Ultra96-V2 is powered down. An alternative would be to clip both the +3.3V and +5V pins on your MIKROE-1985 as the Board is self-powered from the USB. The MIKROE-1985 does not need +5V or +3.3V from the mezzanine.

    Thank you for the great feedback! We will work on getting some more answers.

    Bryan

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    +1 bhfletcher over 4 years ago in reply to bhfletcher

    My contact at MikroElektronika gave me the following information

    Some of the early Click boards were developed without a diode. It was intentionally allowed to power up your board with the peripherals. All recent designs are developed without this feature. The diode is not mandatory, however if you want to protect main board from any unwanted powering from the peripheral, then a diode is the way to go.

    We are working with MikroE so that the next version of the 96Boards Click Mezzanine will have this protection diode on the 5V to prevent backfeeding a 96Boards host with 5V from a Click board that may provide 5V to the Mezzanine.

    If you are designing your own board with a MikroE Click site, then you would also want to consider protection diodes on any power rail that you don't want to backfeed into your board.

    As for the Ultra96-V2, please do NOT leave the USB cable plugged into the MIKROE-1985 when the Ultra96-V2 is powered down unless you clip the power pins on the MIKROE-1985.

    Bryan

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • bhfletcher
    +1 bhfletcher over 4 years ago in reply to bhfletcher

    My contact at MikroElektronika gave me the following information

    Some of the early Click boards were developed without a diode. It was intentionally allowed to power up your board with the peripherals. All recent designs are developed without this feature. The diode is not mandatory, however if you want to protect main board from any unwanted powering from the peripheral, then a diode is the way to go.

    We are working with MikroE so that the next version of the 96Boards Click Mezzanine will have this protection diode on the 5V to prevent backfeeding a 96Boards host with 5V from a Click board that may provide 5V to the Mezzanine.

    If you are designing your own board with a MikroE Click site, then you would also want to consider protection diodes on any power rail that you don't want to backfeed into your board.

    As for the Ultra96-V2, please do NOT leave the USB cable plugged into the MIKROE-1985 when the Ultra96-V2 is powered down unless you clip the power pins on the MIKROE-1985.

    Bryan

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • dqlb
    0 dqlb over 4 years ago in reply to bhfletcher

    Thanks for the detailed replies Bryan. I've gone ahead and clipped the power pins of the MIKROE-1985 click board as that seems like the most robust solution.