Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Can I connect the MpSoC peripherals (uart, DP, Ethernet, SDs, etc) to the PL (without using the PS)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1609 views
  • Users 0 members are here
Related

Can I connect the MpSoC peripherals (uart, DP, Ethernet, SDs, etc) to the PL (without using the PS)

lord_rafa
lord_rafa over 3 years ago

Hello,

I would like to know if it is possible to access the peripherals directly from the PL without running any software on the PS. Would it be this the use of an AXI Slave? if so is there any IP open IP to control the communications with these peripherals?

The reason of asking this is to be able to do one of these things:

  • Read a video input wired to the PL, perform some transformation and output the resulting image to the DP.
  • Do a raw reading directly from the SD port available on the ultra96.
  • Communicate with the PL using the onboard UART on the Ultra96.
  • Use the Ethernet peripheral, generate some traffic from the PL and output the result to a PL IO pin.

I could even use a soft core cpu to implement the drivers but I would like to know till which extension the PS can be ignored and the PL can control elements from the MpSoC

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +1
    This is discussed at the same link I provided on your other question. The answer is on slide 2: https://www.xilinx.com/video/soc/mio-emio-configuration-zynq-7000.html
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to lord_rafa +1
    Maybe try it with one pin? It 'll show reality vs assumption.
  • shabaz
    shabaz over 3 years ago

    This is discussed at the same link I provided on your other question. The answer is on slide 2:

    https://www.xilinx.com/video/soc/mio-emio-configuration-zynq-7000.html

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • lord_rafa
    lord_rafa over 3 years ago in reply to shabaz

    Thank you shabaz. As I can see it is not possible because the controlling interfaces are mapped in PS memory and that would involve that necessarily involved the PS.

    What looks like it is possible is to use EMIO to route the external interface of some of this peripherals and made the external interface available for the PL or the PL pins.

    However what I think I can do is read/write the PS memory from the PL using an AXI IP in the PL, hence I should be able to control the PS peripherals from the PL, Am I right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to lord_rafa

    Maybe try it with one pin? It 'll show reality vs assumption.