Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design VNC server in Petalinux - can't find
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 1566 views
  • Users 0 members are here
Related

VNC server in Petalinux - can't find

rscasny
rscasny over 3 years ago

I have a member who needs some help regarding VNC Server in petaLinux.

He's tried to find the VNC server enabled Image but could not find it.

Can anyone help?

Randall

element14 Community Team

  • Sign in to reply
  • Cancel

Top Replies

  • rajivbishwokarma
    rajivbishwokarma over 3 years ago +2
    I am not sure about prebuilt VNC server enabled image but take a look at the following document (last 2-3 pages). Link: Deephi-DNNDK-tutorial-for-Ultra96_LogicTronix_June_2019.pdf
  • saadtiwana_int
    saadtiwana_int over 3 years ago +2
    If rebuilding the petalinux image is an option, then tigervnc can be enabled in the image. See the amd support ticket details here: VNC remote desktop client on Ultra96 Petalinux (xilinx.com)
Parents
  • shabaz
    shabaz over 3 years ago

    Hi Randall,

    I have not used PetaLinux so cannot comment if there is a pre-built version of a VNC server, but from working with Linux for many years, it's very rare to need such a thing (and the same would apply to PetaLinux).

    Here are three better options:

    (1)  An alternative is to use a SSH client to connect to the device. It is way faster, and more productive. This solves things for command-line applications.

    (2) For the rare occasions that a graphical application needs to run, then there is always the option to run an X server. There is a free one here:

    https://sourceforge.net/projects/vcxsrv/

    and it works very well. This would work with all Linuxes, including PetaLinux, because X is a standard.

    (3) If speedy graphical applications need to be run, then nothing beats a local display monitor connection, e.g. HDMI, if the device has such a connection (VNC is too slow in comparison).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    Hi Randall,

    I have not used PetaLinux so cannot comment if there is a pre-built version of a VNC server, but from working with Linux for many years, it's very rare to need such a thing (and the same would apply to PetaLinux).

    Here are three better options:

    (1)  An alternative is to use a SSH client to connect to the device. It is way faster, and more productive. This solves things for command-line applications.

    (2) For the rare occasions that a graphical application needs to run, then there is always the option to run an X server. There is a free one here:

    https://sourceforge.net/projects/vcxsrv/

    and it works very well. This would work with all Linuxes, including PetaLinux, because X is a standard.

    (3) If speedy graphical applications need to be run, then nothing beats a local display monitor connection, e.g. HDMI, if the device has such a connection (VNC is too slow in comparison).