Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96-V2 Errata
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 378 subscribers
  • Views 9473 views
  • Users 0 members are here
  • ultra96
Related

Ultra96-V2 Errata

bhfletcher
bhfletcher over 7 years ago

We have started shipping Ultra96-V2! There are a few minor issues which I will add to this discussion post. Any future Erratum that are found will also be posted here first, and then added to the Errata document posted under Ultra96-V2 Documentation.

  • Sign in to reply
  • Cancel

Top Replies

  • fuzzynavel
    fuzzynavel over 7 years ago +1
    Hi Bryan: The Quick Start card also references a Getting Started Guide that doesn't yet seem to exist on the V2 Documentation Guild site yet. Probably just not posted yet?
  • bhfletcher
    bhfletcher over 7 years ago in reply to fuzzynavel +1
    Yes, working on it now. Hope to have it posted tonight. We are also working on a new design with the access point working, so that will then require a new download and updated document. Bryan
  • bhfletcher
    bhfletcher over 7 years ago in reply to bhfletcher +1
    A first version of the Getting Started Guide is now posted. We are working on updating the image to fix many of the bugs in the Webserver. Thank you for your patience. The document is posted here: Ultra96…
Parents
  • bhfletcher
    bhfletcher over 7 years ago

    The first 3000 kits include a Quick-Start Card that states no LEDs are lit when powered off. This is not correct. For Revision 1, we added LED D17 which is lit whenever 12V is alive. This was added to remind users that they should not add pods or mezzanines to the board when plugged into 12V, even if the power is off (because it's not really off until you unplug the barrel jack!).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bhfletcher
    bhfletcher over 7 years ago

    The first 3000 kits include a Quick-Start Card that states no LEDs are lit when powered off. This is not correct. For Revision 1, we added LED D17 which is lit whenever 12V is alive. This was added to remind users that they should not add pods or mezzanines to the board when plugged into 12V, even if the power is off (because it's not really off until you unplug the barrel jack!).