Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Error in building mult example using Avnet UltraZed-EG Starter Kit (SOM and Carrier Card)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 361 subscribers
  • Views 1838 views
  • Users 0 members are here
Related

Error in building mult example using Avnet UltraZed-EG Starter Kit (SOM and Carrier Card)

fasih.ahmed
fasih.ahmed over 7 years ago

Dear All,

 

I am facing problem in running simple Mult example in SDx. I have also try to change the folder name of the BDF but does not work as mention in this link Ultra96 SDSoC 2018.2 Platform Install | Zedboard

Please, if you have any solution to this problem then let me know.

I am using Xilinx Sdx 2018.2 with

 

 

 

===>The following messages were generated while creating FPGA bitstream. Log file:/home/ahmed/Xilinx2018.2/SDx/2018.2/workspace-2018.2/MM-test/Debug/_sds/p0/vivado/vivado.log :

ERROR: [VPL 49-71] The board_part definition was not found for em.avnet.com:ultrazed_eg_pciecc_production:part0:1.1. The project's board_part property was not set, but the project's part property was set to xczu3eg-sfva625-1-i. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.

ERROR: [VPL 60-773] In '/home/ahmed/Xilinx2018.2/SDx/2018.2/workspace-2018.2/MM-test/Debug/_sds/p0/vivado/vivado.log', caught Tcl error:  ERROR: [Board 49-71] The board_part definition was not found for em.avnet.com:ultrazed_eg_pciecc_production:part0:1.1. The project's board_part property was not set, but the project's part property was set to xczu3eg-sfva625-1-i. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.

ERROR: [VPL 60-704] Integration error, problem rebuilding project prj

ERROR: [VPL 60-806] Failed to finish platform linker

ERROR: [SdsCompiler 83-5019] Exiting sds++ : Error when calling '/home/ahmed/Xilinx2018.2/SDx/2018.2/bin/vpl   --iprepo /home/ahmed/Xilinx2018.2/SDx/2018.2/workspace-2018.2/MM-test/Debug/_sds/iprepo/repo  --iprepo /home/ahmed/Xilinx2018.2/SDx/2018.2/data/ip/xilinx  --platform /home/ahmed/Xilinx2018.2/SDx/2018.2/platforms/uzegpcie_avnet/uzegpcie_avnet.xpfm  --temp_dir /home/ahmed/Xilinx2018.2/SDx/2018.2/workspace-2018.2/MM-test/Debug/_sds/p0  --output_dir /home/ahmed/Xilinx2018.2/SDx/2018.2/workspace-2018.2/MM-test/Debug/_sds/p0/vpl  --input_file /home/ahmed/Xilinx2018.2/SDx/2018.2/workspace-2018.2/MM-test/Debug/_sds/p0/.xsd/top.bd.tcl  --target hw   --save_temps  --kernels mmult_accel:adapter --webtalk_flag SDSoC  --remote_ip_cache /home/ahmed/Xilinx2018.2/SDx/2018.2/workspace-2018.2/ip_cache --xp "param:compiler.deleteDefaultReportConfigs=false" '

sds++ log file saved as /home/ahmed/Xilinx2018.2/SDx/2018.2/workspace-2018.2/MM-test/Debug/_sds/reports/sds.log

ERROR: [SdsCompiler 83-5004] Build failed

 

Thanks,

Ahmed

  • Sign in to reply
  • Cancel

Top Replies

  • drozwood90
    drozwood90 over 7 years ago in reply to clem57 +1
    Clem57, Check this link for other links and information on BDF (Board Definition File) Basically lets someone define a board - useful if you have a standard product you use a lot. https://forums.xilinx…
  • drozwood90
    drozwood90 over 7 years ago

    You need to install the BDF files per this link:

     

    https://github.com/Avnet/bdf

     

    Without the BDF, the system cannot understand what to do. 

     

    The specific one you need is

    ultrazed_3eg_pciecc/1.1/

    em.avnet.com:ultrazed_eg_pciecc_production:part0:1.1

    Listed under https://github.com/Avnet/bdf/tree/master/

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to drozwood90

    Just what is the BDF and what is it for?

    Thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fasih.ahmed
    fasih.ahmed over 7 years ago in reply to drozwood90

    Thanks, Dan !

    I have already install BDF in /home/ahmed/Xilinx2018.2/Vivado/2018.2/data/boards/board_files

    Btw what's a difference between this two links ....looks similar to me

    Thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jafoste4
    jafoste4 over 7 years ago in reply to fasih.ahmed

    hi,

     

    What BDF version did you install?

     

    Thx,
    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fasih.ahmed
    fasih.ahmed over 7 years ago in reply to jafoste4

    Hi josh,

     

    1.0 version

     

    Thnx

     

    Ahmed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jafoste4
    jafoste4 over 7 years ago in reply to fasih.ahmed

    It wants you to install the 1.1 version.

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • drozwood90
    drozwood90 over 7 years ago in reply to clem57

    Clem57,

     

    Check this link for other links and information on BDF (Board Definition File)

    Basically lets someone define a board - useful if you have a standard product you use a lot.

     

    https://forums.xilinx.com/t5/Design-Entry/Board-definition-file-in-Vivado/td-p/496384

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fasih.ahmed
    fasih.ahmed over 7 years ago in reply to jafoste4

    Hi Josh,

     

    Thanks got your point

     

    BR,

    Ahmed