Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Since SD1/WP of board definition file is not set to MIO44, SD card is write protected.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 491 views
  • Users 0 members are here
Related

Since SD1/WP of board definition file is not set to MIO44, SD card is write protected.

ikwzm
ikwzm over 8 years ago

I also met the same kind of trouble as this thread.

http://zedboard.org/content/issues-loading-rootfs-sd-card

This thread avoids the problem by setting "disable-wp" to devicetree.

However, this problem does not exist in the board difinition file, "I / O Configuration"> "Low Speed"> "Memory Interfaces"> "SD"> "SD 1"> "WP" is not set Is the cause
 
I suggest adding the following description to the board difinition file (ultrazed_3eg_iocc/1.0/preset.xml).
 
<user_parameter name = "CONFIG.PSU__SD1__GRP_WP__ENABLE" value = "1" />
<user_parameter name = "CONFIG.PSU__SD1__GRP_WP__IO" value = "MIO 44" />
 
Is there any problem with this method?
 
  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    UltraZed IO Carrier Card uses microSD card and there is no WP pin for microSD card slots (only standard SD card uses the WP pin). So, there is no need to define a WP pin for the IOCC in the board definition files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ikwzm
    0 ikwzm over 8 years ago in reply to e14 Contributor

    "UltraZed I/O Carrer Card Version 1.0"  Page20  - 2.8 PS microSD Card Connector – J4

    http://zedboard.org/sites/default/files/documentations/UltraZed%20IOCC-UG%201v1-1.pdf

    According to this document, MIO 44 is connected to SD_WP(JP2). Is it necessary to set board diffinition file?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • micahstevens
    0 micahstevens over 8 years ago in reply to e14 Contributor

    The OS will still look for it though, and it's connected to the jumper on the board. This is necessary unless you disable the WP functionality.