Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Ultrazed SOM USB interface - Power required if not using USB?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 327 views
  • Users 0 members are here
Related

Ultrazed SOM USB interface - Power required if not using USB?

400garrison
400garrison over 8 years ago

If we don’t want to use the USB interface on the UltraZed SOM, do we still have to provide power to it?

Thanks,

Adam

  • Sign in to reply
  • Cancel
  • ctammann
    0 ctammann over 8 years ago

    I assume you are referring to the 5V for USB_VBUS? If you are not using the interface you should not have to provide this voltage, although I haven't tested this myself. USB VBUS is only used to determine operating mode. The other supplies for the USB device are shared on the bank voltages so those would be needed even if you didn't use USB. To be on the safe side you could always hold the device in reset using the P1_USB0_RST_N signal, that way the device is tristated anyway. I'm a little out of my zone here, but I believe you can drive that signal from the I/O expander using the I2C bus