Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Is power management possible on Ultrazed-EG?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 362 subscribers
  • Views 748 views
  • Users 0 members are here
Related

Is power management possible on Ultrazed-EG?

rda_emcraft
rda_emcraft over 9 years ago

We are looking for a hardware platform to prototype power management on Zynq.

We need the hardware to be started with only Low-Power Domain and PS MIO powered on Zynq with the ability to turn of Full-Power and Programming Logic power domains later under software control.  Is this possible on Ultrazed-EG?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    UltraZed-EG SOM power is designed to allow entring low power mode after the initial power-on. What that means is that the SOM will always power-on in Full Power Mode and then it can be placed in the Low Power Mode under software control.

    The UltraZed-EG SOM power rails are implemented using two Infineon PMIC devices. The PMIC devices can be controlled via their PMBus interface for the purpose of power management. Using the PMBus interface, any PMIC output voltage can be turned off under software control. On the UltraZed-EG SOM the PMIC PMBus interface is connected to the MPSoC I2C interface (PS MIO pins that are always powered). This allows software to control the PMIC devices via the MPSoC I2C interface and turn off some of the PMIC outputs on demand.

    In April, we will post a reference design on ultrazed.org website that will demonstrate the Low Power Mode capabilities of the UltraZed-EG SOM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    UltraZed-EG SOM power is designed to allow entring low power mode after the initial power-on. What that means is that the SOM will always power-on in Full Power Mode and then it can be placed in the Low Power Mode under software control.

    The UltraZed-EG SOM power rails are implemented using two Infineon PMIC devices. The PMIC devices can be controlled via their PMBus interface for the purpose of power management. Using the PMBus interface, any PMIC output voltage can be turned off under software control. On the UltraZed-EG SOM the PMIC PMBus interface is connected to the MPSoC I2C interface (PS MIO pins that are always powered). This allows software to control the PMIC devices via the MPSoC I2C interface and turn off some of the PMIC outputs on demand.

    In April, we will post a reference design on ultrazed.org website that will demonstrate the Low Power Mode capabilities of the UltraZed-EG SOM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    I am trying to marginally change the core voltage of PL marginally (+- 3 % probably). May I know the names of those Infineon's PMBus interface software and dongle?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rda_emcraft
    0 rda_emcraft over 9 years ago in reply to e14 Contributor

    Are there any news on that reference design with Low Power Mode?

    I was unable to find it on the site.