Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design No QEMU hardware DTS or prebuilt DTB found
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 1750 views
  • Users 0 members are here
Related

No QEMU hardware DTS or prebuilt DTB found

pgielmuda
pgielmuda over 8 years ago

Hi,

I would like to run petlinux on Ultrazed EG IO Carrier Card. I use bsp from: 

http://ultrazed.org/support/design/17956/141

However I have some problems with that and I would like to test it on my PC before I download it to hardware. I try to run qemu emulator with command:

petalinux-boot --qemu --kernel 

After that I got en error:

ERROR: No QEMU hardware DTS or prebuilt DTB found. This is required to boot ZynqMP on QEMU

In the <design_folder>/pre-build/linux/images I have a file: zynqmp-qemu-arm.dtb.

In the <design_folder>/images/linux I do not any *qemu*.dts file. How to fix that?

I suppose that I do not enable/include qemu options/files in the build process but I do not know how to do that.

  • Sign in to reply
  • Cancel
  • pgielmuda
    0 pgielmuda over 8 years ago

    I found that I can run pre-build images with the command:

    petalinux-boot --qemu --prebuild 3

    In such case I have two problems:

    WARNING: Failed to load PMUFW, doesn't exist in prebuilts.See help to load custom PMUFW
    ERROR: No QEMU hardware DTS or prebuilt DTB found. This is required to boot ZynqMP on QEMU
     
    I could copy pmufw.elf from generated files (<design_folder>/images/linux) but still there is a problem with DTS/DTB files even for prebuilt images. 
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 8 years ago

    Hello,

    This is a known issue that is described here:

    https://forums.xilinx.com/t5/Embedded-Development-Tools/ERROR-No-QEMU-hardware-DTS-or-prebuilt-DTB-found-This-is/td-p/758765

    The zynqmp-qemu-arm.dtb file needs to be in the <petalinux_project_folder>/images/linux folder.

    In general the Xilinx forums will be a much better site to search for answers and ask questions related to the Xilinx Vivado and PetaLinux tools.

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • a.ineo
    0 a.ineo over 8 years ago

    Same problem with an Ultrazed-EG.

    I tested with the BSP from Avnet and with my custom hdf.

    petalinux-create -t project -s ~/uz3eg_iocc_2017_2.bsp
    cd ./uz3eg_iocc_2017_2
    petalinux-build
     
    Copy "zynqmp-qemu-arm.dtb" in <petalinux_project_folder>/images/linux folder.
     
      petalinux-boot --qemu --prebuild 3
      ERROR: No QEMU hardware DTS or prebuilt DTB found. This is required to boot ZynqMP on QEMU