Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design DDR I/O not in the Ultrazed design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 596 views
  • Users 0 members are here
Related

DDR I/O not in the Ultrazed design

sonictai
sonictai over 9 years ago

Hello,

I have followed the UltraZed EG Starter Kit Tutorial (for the 2016.4 Vivado version) to recreate the demo project, everything's OK, I am able to synthese and implement the design but when I open the implemented design there are no DDR and MIO I/O mapped to any pads!!

When I generate the block design there is no DDR port (in a Zynq 7000 project this DDR port appears), so the wrapper has no DDR interface, and then the design doesn't contains DDR interface!

Where are those DDR and MIO signals defined in the project? Not in any xdc file...is it normal that the DDR port isn't in the BD?

Thank you, Christophe

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Staring with MPSoC family, the PS dedicated pins such as DDR and MIO are no longer shown in the block design or in "implemented design" as these pins are not user defined in the top-level XDC file. You also won't see these ports in the top-level wrapper file. But rest asure, these pins are connected to the MPSoC external devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sonictai
    0 sonictai over 9 years ago in reply to e14 Contributor

    Thank you for your fast response. However I was expecting to find them in the "package pins" part of the implemented design!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to sonictai

    You can view these pins in the Vivado IO Report.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer