Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Ultrazed USB Device Mode
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 360 subscribers
  • Views 747 views
  • Users 0 members are here
Related

Ultrazed USB Device Mode

adiaz04
adiaz04 over 8 years ago

How do I put the Ultrazed SOM/IO carrier combo in USB Device Mode?

My goal is to be able to connect the board to a PC and access the eMMC.

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Is your intentions to just set the hardware to device mode and then see it on your PC? (No applications running)

    From my limited knowledge in this area, In a standalone enviroment I had to run an application to setup in my case a PicoZed to where I could view it from my windows PC/write to it.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • adiaz04
    0 adiaz04 over 8 years ago in reply to jafoste4

    Hi Josh - my ultimate goal is to be able to format and partition the eMMC without having to boot into linux on the device. I figued I might be able to put the board in device mode so that the pc can just see the eMMC as an external usb drive or something which would allow me to format the eMMC from my pc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dyessgg
    0 dyessgg over 8 years ago in reply to adiaz04

    You would need firmware running on the UltraZed to implement USB MSC class to respond to the USB  commands from the host.  There's no automagic passthrough from USB to eMMC.  That would all have to be done via firmware running on the processor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dyessgg
    0 dyessgg over 8 years ago in reply to adiaz04

    You would need firmware running on the UltraZed to implement USB MSC class to respond to the USB  commands from the host.  There's no automagic passthrough from USB to eMMC.  That would all have to be done via firmware running on the processor.