Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed SD Boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 1229 views
  • Users 0 members are here
Related

UltraZed SD Boot

e14 Contributor
e14 Contributor over 9 years ago

Xilinx Tool Chain Version: 2016.2

I am currently in the process of recreating the OOBE for the UltraZed IOCC. I have successfully rebuilt the OOBE running the commands manually and applying the configurations/patch files found on Avnet's Github: https://github.com/Avnet/software 

The problem is I am trying to change the rootfs from the RAMFS to the SD Card. In the Petalinux Generic Config File I have changed the Image Packaging Configuration to the following:

# Image Packaging Configuration
#
# CONFIG_SUBSYSTEM_ROOTFS_INITRAMFS is not set
# CONFIG_SUBSYSTEM_ROOTFS_INITRD is not set
# CONFIG_SUBSYSTEM_ROOTFS_JFFS2 is not set
# CONFIG_SUBSYSTEM_ROOTFS_NFS is not set
CONFIG_SUBSYSTEM_ROOTFS_SD=y
# CONFIG_SUBSYSTEM_ROOTFS_OTHER is not set
CONFIG_SUBSYSTEM_SDROOT_DEV="/dev/mmcblk1p2"
CONFIG_SUBSYSTEM_UIMAGE_NAME="image.ub"
# CONFIG_SUBSYSTEM_UIMAGE_HASH_NONE is not set
CONFIG_SUBSYSTEM_UIMAGE_HASH_CRC32=y
# CONFIG_SUBSYSTEM_UIMAGE_HASH_SHA1 is not set
# CONFIG_SUBSYSTEM_UIMAGE_HASH_BOTH is not set
CONFIG_SUBSYSTEM_COMPRESS_IMAGE=y
CONFIG_SUBSYSTEM_DTB_PADDING_SIZE=0x1000
# CONFIG_SUBSYSTEM_COPY_TO_TFTPBOOT is not set

And the Kernel BootArgs:

CONFIG_SUBSYSTEM_BOOTARGS_GENERATED="earlycon=cdns,mmio,0xFF000000,115200n8 root=/dev/mmcblk1p2 rw rootdelay=2 rootfstype=ext4"

In the Device Tree, system-conf.dtsi I modified the bootargs:

chosen {
bootargs = "earlycon=cdns,mmio,0xFF000000,115200n8 root=/dev/mmcblk1p2 rw rootdelay=2 rootfstype=ext4";
stdout-path = "serial0:115200ns";
};

 

Rebuilding with only those changes is causing the Kernel to hang when booting:

U-Boot 2016.01 (Feb 01 2017 - 15:35:26 -0500)
DRAM:  2 GiB
Enabling Caches...
EL Level:       EL2
MMC:   sdhci@ff160000: 0, sdhci@ff170000: 1
Invalid bus 0 (err=-19)
*** Warning - spi_flash_probe() failed, using default environment

## Error: flags type check failure for "serverip" <= "AUTO" (type: i)
himport_r: can't insert "serverip=AUTO" into hash table
In:    serial
Out:   serial
Err:   serial
Bootmode: SD_MODE1
Net:   ZYNQ GEM: ff0e0000, phyaddr 5, interface rgmii-id
eth0: ethernet@ff0e0000

U-BOOT for Linux

Hit any key to stop autoboot:  0
Device: sdhci@ff160000
Manufacturer ID: 13
OEM: 14e
Name: Q2J55
Tran Speed: 52000000
Rd Block Len: 512
MMC version 5.0
High Capacity: Yes
Capacity: 7.1 GiB
Bus Width: 8-bit
Erase Group Size: 512 KiB
HC WP Group Size: 8 MiB
User Capacity: 7.1 GiB WRREL
Boot Capacity: 16 MiB ENH
RPMB Capacity: 4 MiB ENH
reading image.ub
5312456 bytes read in 370 ms (13.7 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
   Using 'conf@1' configuration
   Trying 'kernel@1' kernel subimage
     Description:  PetaLinux Kernel
     Type:         Kernel Image
     Compression:  gzip compressed
     Data Start:   0x100000f4
     Data Size:    5283581 Bytes = 5 MiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x00080000
     Entry Point:  0x00080000
     Hash algo:    crc32
     Hash value:   962d8cfa
   Verifying Hash Integrity ... crc32+ OK
## Loading fdt from FIT Image at 10000000 ...
   Using 'conf@1' configuration
   Trying 'fdt@1' fdt subimage
     Description:  Flattened Device Tree blob
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0x1050a0dc
     Data Size:    27564 Bytes = 26.9 KiB
     Architecture: AArch64
     Hash algo:    crc32
     Hash value:   8891f2ad
   Verifying Hash Integrity ... crc32+ OK
   Booting using the fdt blob at 0x1050a0dc
   Uncompressing Kernel Image ... OK
   Loading Device Tree to 0000000007ff6000, end 0000000007fffbab ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.4.0 (rshumate@ip-172-31-62-121.ec2.internal) (gcc version 4.9.2 20140904 (prerelease) (crosstool-NG linaro-1.13.1-4.9-2014.09 - Linaro GCC 4.9-2014.09) ) #1 SMP Wed Feb 1 15:33:48 EST 2017
[    0.000000] Boot CPU: AArch64 Processor [410fd034]
[    0.000000] earlycon: Early serial console at MMIO 0xff000000 (options '115200n8')
[    0.000000] bootconsole [uart0] enabled
[    0.000000] cma: Reserved 128 MiB at 0x0000000078000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.0 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] PERCPU: Embedded 16 pages/cpu @ffffffc077f8e000 s24704 r8192 d32640 u65536
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 517120
[    0.000000] Kernel command line: earlycon=cdns,mmio,0xFF000000,115200n8 root=/dev/mmcblk1p2 rw rootdelay=2
[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)
[    0.000000] software IO TLB [mem 0x71e00000-0x75e00000] (64MB) mapped at [ffffffc071e00000-ffffffc075dfffff]
[    0.000000] Memory: 1856664K/2097152K available (7198K kernel code, 520K rwdata, 2748K rodata, 280K init, 356K bss, 109416K reserved, 131072K cma-reserved)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vmalloc : 0xffffff8000000000 - 0xffffffbdffff0000   (   247 GB)
[    0.000000]     vmemmap : 0xffffffbe00000000 - 0xffffffbfc0000000   (     7 GB maximum)
[    0.000000]               0xffffffbe00000000 - 0xffffffbe01c00000   (    28 MB actual)
[    0.000000]     fixed   : 0xffffffbffa7fd000 - 0xffffffbffac00000   (  4108 KB)
[    0.000000]     PCI I/O : 0xffffffbffae00000 - 0xffffffbffbe00000   (    16 MB)
[    0.000000]     modules : 0xffffffbffc000000 - 0xffffffc000000000   (    64 MB)
[    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc080000000   (  2048 MB)
[    0.000000]       .init : 0xffffffc000a38000 - 0xffffffc000a7e000   (   280 KB)
[    0.000000]       .text : 0xffffffc000080000 - 0xffffffc000a37044   (  9949 KB)
[    0.000000]       .data : 0xffffffc000a90000 - 0xffffffc000b12160   (   521 KB)
[    0.000000] Hierarchical RCU implementation.
[    0.000000]  Build-time adjustment of leaf fanout to 64.
[    0.000000]  RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4
[    0.000000] NR_IRQS:64 nr_irqs:64 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] Architected cp15 timer(s) running at 100.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
[    0.000004] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
[    0.008362] Console: colour dummy device 80x25
[    0.012618] console [tty0] enabled
[    0.015983] bootconsole [uart0] disabled
 
Any help solving this would be greatly appreciated!
Thanks,
Ryan 
 
 
 
  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 9 years ago

    Hi Ryan,

    The issue you are experiencing sounds like it is related to the issue reported in this Xilinx thread:

    https://forums.xilinx.com/t5/Embedded-Linux/Petalinux-2016-4-boot-from-SD-with-ext4-rootfs/td-p/742310

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to zedhed

    Thanks Kevin for the suggestion.

    I rebuilt everything moving the device tree to the SD Card and it is still hanging at the same place. I am using a custom file system on the second partition, but from my understanding of where it is hanging at, whether the file system is good or not should not be an issue. The next part of the boot order should be the Kernel starting all 4 of the CPUs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to zedhed

    Thanks Kevin for the suggestion.

    I rebuilt everything moving the device tree to the SD Card and it is still hanging at the same place. I am using a custom file system on the second partition, but from my understanding of where it is hanging at, whether the file system is good or not should not be an issue. The next part of the boot order should be the Kernel starting all 4 of the CPUs.