Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Xen Hypervisor on UltraZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 362 subscribers
  • Views 709 views
  • Users 0 members are here
Related

Xen Hypervisor on UltraZed

rsk_hayashi
rsk_hayashi over 8 years ago

Hello,

 

I'm trying to boot up Xen on UltraZed-EG Starter Kit.

Petalinux 2017.2 works with the new BSP file.

Then, I tried to build Xen for the board according to the link below.

http://www.wiki.xilinx.com/Building+the+Xen+Hypervisor+with+PetaLinux+2017.1

 

It says that "xen-overlay.dtsi" is required, but Petalinux project of UltraZed does not have.

So I would like to ask:

  1.   Is it possible that self-coding the dtsi file?
     
      Is there reference document for Xen dtsi file?
  2.   Do you have a plan to provide the dtsi file for Xen just as ZCU102 board has.

 

Thank you.

Ryosuke

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 8 years ago

    Hi Ryosuke,

    We do not currently have a way to support Xen on UltraZed.  However, I don't know of any reason why you should not be able to get this to work.

    According to this post, you can just copy xen-overlay.dtsi from a ZCU102 BSP and modify according to your settings.

    https://forums.xilinx.com/t5/Embedded-Linux/Petalinux-2017-2-Failed-to-create-xen-overlay-dtsi/td-p/797358

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jarvisroach
    0 jarvisroach over 8 years ago

    We are working on a Yocto recipe of our Xen distribution to support the UltraZed board. We have it up an running and will be pushing it out to github soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • harias
    0 harias over 8 years ago in reply to jarvisroach

    Hi Jarvis, 

    I am also testing the UltraZed board:

    http://zedboard.org/product/ultrazed-eg-starter-kit

     

    So, is there a place where we can monitor the release of the Yocto recipe you mentioned? Or, can you send me a copy of the draft? We are in the middle of a prototype and really need Xen on UltraZed to complete it.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sivatt
    0 sivatt over 8 years ago in reply to zedhed

    Hello Kevin,

    I have taken xen-overlay.dtsi and build the boot image as per http://www.wiki.xilinx.com/Building%20the%20Xen%20Hypervisor%20with%20PetaLinux%202017.3 with SD card.

    Target got booted. but i am getting error while trying "To start a simple guest run the following from the dom0 prompt". 

    root@hypervisor:/etc/xen# xl create example-simple.cfg 

    Parsing config from example-simple.cfg
    xc: error: panic: xc_dom_core.c:208: failed to open file '/boot/Image': No such file or directory: Internal error
    libxl: error: libxl_dom.c:709:libxl__build_pv: xc_dom_kernel_file failed: No such file or directory
    libxl: error: libxl_create.c:1223:domcreate_rebuild_done: cannot (re-)build domain: -3
    libxl: error: libxl.c:1575:libxl__destroy_domid: non-existant domain 1
    libxl: error: libxl.c:1534:domain_destroy_callback: unable to destroy guest with domid 1
    libxl: error: libxl.c:1463:domain_destroy_cb: destruction of domain 1 failed

    Please let me know if you have any suggestions. (I am using 2017.4 petalinux tools)

    Thanks,

    Siva