Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed EG not booting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 1285 views
  • Users 0 members are here
Related

UltraZed EG not booting

xlmnsp
xlmnsp over 8 years ago

I am having some problems getting my UltraZed EG starter kit to boot. 

I've followed all of the quick start steps and inserted the supplied SD card. The fan is working.

 

After turning on the board, D10 on the carried board lights up and D15 on the carried board stays dark.

 

D4 on the SOM flashes and if the boot mode is set to SD, D3 on the SOM lights up continously. If the boot mode is set to one of the QSPI modes the SOM stays dark after the D4 flash. Except in some cases if I leave the board on for a while, D3 turns on.

 

Nothing shows up on the serial connection.

 

I hope this description helps with identifying the problem. I would greatly appreciate any help.

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 8 years ago

    Hi there,

    That was a good idea to try to connect both. Typically it is the HIGHER port number. For example, on my PC (running Windows 10), I have ports 5 and 6 for serial ports. 6 happens to be the one I need to use to see the terminal.

    Just a few more questions to help me understand, and I am sorry if they seem annoying or simple.
    *are you in fact using 115,200/8N1 for your serial terminal (we did not confirm this)?
    *are you using Tera Term?
    *can you look at your boot switch matrix and tell me what the switches are set to?
    The switch is labeled 1-4 and one side should say ON.

    For example, you can write it like this:
    1   2   3   4
    OFF ON  ON  ON

    NOTE: this configuration will boot from the built in QSPI, and load the factory loaded code (unless you have overwritten it).

    If you have NOT seen it, other boot configurations are in the SOM manual on page 32.

    For example, SDCARD Boot is:
    1   2   3   4
    OFF ON  OFF ON

    While we are gathering information, can you try the two above configurations? First, try the FIRST example Matrix setup.

    Next delete all files and folders from the included SDCARD.  Ensure it is the INCLUDED SDCARD.  If it is not, this could be your issue (see Storage Insights Article on Element 14).
    Next, extract ONLY the BOOT.BIN and image.ub to the SDCARD.  Place this in the Carrier Card and change the boot switch matrix configuration to the SDCARD boot.

    Power each on one at a time and please let me know what you see.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 8 years ago

    Hi there,

    That was a good idea to try to connect both. Typically it is the HIGHER port number. For example, on my PC (running Windows 10), I have ports 5 and 6 for serial ports. 6 happens to be the one I need to use to see the terminal.

    Just a few more questions to help me understand, and I am sorry if they seem annoying or simple.
    *are you in fact using 115,200/8N1 for your serial terminal (we did not confirm this)?
    *are you using Tera Term?
    *can you look at your boot switch matrix and tell me what the switches are set to?
    The switch is labeled 1-4 and one side should say ON.

    For example, you can write it like this:
    1   2   3   4
    OFF ON  ON  ON

    NOTE: this configuration will boot from the built in QSPI, and load the factory loaded code (unless you have overwritten it).

    If you have NOT seen it, other boot configurations are in the SOM manual on page 32.

    For example, SDCARD Boot is:
    1   2   3   4
    OFF ON  OFF ON

    While we are gathering information, can you try the two above configurations? First, try the FIRST example Matrix setup.

    Next delete all files and folders from the included SDCARD.  Ensure it is the INCLUDED SDCARD.  If it is not, this could be your issue (see Storage Insights Article on Element 14).
    Next, extract ONLY the BOOT.BIN and image.ub to the SDCARD.  Place this in the Carrier Card and change the boot switch matrix configuration to the SDCARD boot.

    Power each on one at a time and please let me know what you see.

    --Dan