Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed EG not booting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 1284 views
  • Users 0 members are here
Related

UltraZed EG not booting

xlmnsp
xlmnsp over 8 years ago

I am having some problems getting my UltraZed EG starter kit to boot. 

I've followed all of the quick start steps and inserted the supplied SD card. The fan is working.

 

After turning on the board, D10 on the carried board lights up and D15 on the carried board stays dark.

 

D4 on the SOM flashes and if the boot mode is set to SD, D3 on the SOM lights up continously. If the boot mode is set to one of the QSPI modes the SOM stays dark after the D4 flash. Except in some cases if I leave the board on for a while, D3 turns on.

 

Nothing shows up on the serial connection.

 

I hope this description helps with identifying the problem. I would greatly appreciate any help.

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 8 years ago

    Hi there,

    Are you using Windows 10?
    If so, sometimes you will see multiple serial ports appearing.  Can you check your serial settings and ensure you are on the actual serial port?  FYI, both will have a port number assigned.  You can try the second port to see if this is the issue.

    Is your board a red or black?

    When set to SD mode, D3 indicates that there is something wrong with your SDCARD boot.bin.  You should attempt to copy a new one from the resources page.

    In come cases, the boot will time out if you have not accessed it and D3 can light.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • xlmnsp
    0 xlmnsp over 8 years ago in reply to drozwood90

    Hi, thanks for the help,

    Yes I'm using Windows 10.

     

    Since I wasn't sure which serial connection was the correct one, I always had both connected at once. Now I also tried just being connected to one at a time. I also double checked the configuration in both Windows and PuTTY. Still nothing sadly.

     

    My board is black.

     

    I downloaded this file and copied its extracted contents to the root of my SD card http://www.ultrazed.org/sites/default/files/design/uz3eg_iocc_oob_plnx_2017_2.zip. This didn't change anything about the boot behavior.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • xlmnsp
    0 xlmnsp over 8 years ago in reply to drozwood90

    Hi, thanks for the help,

    Yes I'm using Windows 10.

     

    Since I wasn't sure which serial connection was the correct one, I always had both connected at once. Now I also tried just being connected to one at a time. I also double checked the configuration in both Windows and PuTTY. Still nothing sadly.

     

    My board is black.

     

    I downloaded this file and copied its extracted contents to the root of my SD card http://www.ultrazed.org/sites/default/files/design/uz3eg_iocc_oob_plnx_2017_2.zip. This didn't change anything about the boot behavior.