Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Programming FPGA problem- bitstream is not compatible with the target revision
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 6522 views
  • Users 0 members are here
Related

Programming FPGA problem- bitstream is not compatible with the target revision

pgielmuda
pgielmuda over 8 years ago

Hi,

I'm doing UltraZed PCIe Carrier Card Tutorial on Vivado V2017.2. Everything went pretty well. I've generated bitsream with vivado and run all off programs till I stucked on 9.3 chapter where I need to program FPGA with generated bitstream. In the SDK there is an error:


09:49:27 ERROR : bitstream is not compatible with the target revision, use -no-revision-check to allow programming

 

When I've tried to program the device with Vivado and I got such error:

 

ERROR: [Labtools 27-3303] Incorrect bitstream assigned to device. Bitstream was generated for part xczu3eg-sfva625-1-i-es1, target device (with IDCODE revision 1) is compatible with production revision bitstreams.
To allow the bitstream to be programmed to the device, use "set_param xicom.use_bitstream_version_check false" tcl command.
 
What does it mean and how to solve it. 
  • Sign in to reply
  • Cancel
Parents
  • pgielmuda
    0 pgielmuda over 8 years ago

    Ok, I've managed to program the device with the Vivado. I used proposed tcl command:
    set_param xicom.use_bitstream_version_check false

    and then program the device with the bitstream.

    Now in the SDK I do not program the FPGA and just run the software. The first run of software gives reasonable outcome. I get proper messages from COM port. However if I want to:
    - run the software second time there is an error:

    Error while launching program: 
    Memory write error at 0x0. Cannot read sctlr_el3. Cannot read r0. Instruction transfer timeout
     
    - program the FPGA with vivado there is an error:
    ERROR: [Labtools 27-3165] End of startup status: LOW
    I need to reset whole board to get proper outcome of software another time.  
     
     
    Based on that I have few questions:
    1. do usage of tcl command: set_param xicom.use_bitstream_version_check false is justified, safe and do not influence proper work of MPSoC?
    2. how to apply this command to SDK so that I could program the FPGA from SDK?
    3. should I worry about errors which are in this post above?
    4. is there a way to set up environment (SDK or Vivado) to not encounter all of this problems in the future (to solve the reason of it not just apply the path command)? 
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pgielmuda
    0 pgielmuda over 8 years ago

    Ok, I've managed to program the device with the Vivado. I used proposed tcl command:
    set_param xicom.use_bitstream_version_check false

    and then program the device with the bitstream.

    Now in the SDK I do not program the FPGA and just run the software. The first run of software gives reasonable outcome. I get proper messages from COM port. However if I want to:
    - run the software second time there is an error:

    Error while launching program: 
    Memory write error at 0x0. Cannot read sctlr_el3. Cannot read r0. Instruction transfer timeout
     
    - program the FPGA with vivado there is an error:
    ERROR: [Labtools 27-3165] End of startup status: LOW
    I need to reset whole board to get proper outcome of software another time.  
     
     
    Based on that I have few questions:
    1. do usage of tcl command: set_param xicom.use_bitstream_version_check false is justified, safe and do not influence proper work of MPSoC?
    2. how to apply this command to SDK so that I could program the FPGA from SDK?
    3. should I worry about errors which are in this post above?
    4. is there a way to set up environment (SDK or Vivado) to not encounter all of this problems in the future (to solve the reason of it not just apply the path command)?