Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Programming FPGA problem- bitstream is not compatible with the target revision
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 6520 views
  • Users 0 members are here
Related

Programming FPGA problem- bitstream is not compatible with the target revision

pgielmuda
pgielmuda over 8 years ago

Hi,

I'm doing UltraZed PCIe Carrier Card Tutorial on Vivado V2017.2. Everything went pretty well. I've generated bitsream with vivado and run all off programs till I stucked on 9.3 chapter where I need to program FPGA with generated bitstream. In the SDK there is an error:


09:49:27 ERROR : bitstream is not compatible with the target revision, use -no-revision-check to allow programming

 

When I've tried to program the device with Vivado and I got such error:

 

ERROR: [Labtools 27-3303] Incorrect bitstream assigned to device. Bitstream was generated for part xczu3eg-sfva625-1-i-es1, target device (with IDCODE revision 1) is compatible with production revision bitstreams.
To allow the bitstream to be programmed to the device, use "set_param xicom.use_bitstream_version_check false" tcl command.
 
What does it mean and how to solve it. 
  • Sign in to reply
  • Cancel
Parents
  • pgielmuda
    0 pgielmuda over 8 years ago

    Yes you are right. However the reason of problem was associated with the board definition that you give with tutorial packs. The are only ES versions. I used them as default input and didn't know that there are any production version definition board. Maybe it is worth to add all of those board definition to tutorial pack? For people who starts their work with these boards it could be much easier to find appropriate one  :). 

    Regards. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pgielmuda
    0 pgielmuda over 8 years ago

    Yes you are right. However the reason of problem was associated with the board definition that you give with tutorial packs. The are only ES versions. I used them as default input and didn't know that there are any production version definition board. Maybe it is worth to add all of those board definition to tutorial pack? For people who starts their work with these boards it could be much easier to find appropriate one  :). 

    Regards.