Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Having problems running apps out of DRAM on the 7EV SOM
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 360 subscribers
  • Views 824 views
  • Users 0 members are here
Related

Having problems running apps out of DRAM on the 7EV SOM

wchase
wchase over 8 years ago

My app runs in OCM, but not out of DDR.  Are there any known problems with the DDR settings in the current Board File for the 7EV SOM?   Are there any recent/penidng board file updates?  FYI: I'm running the SOM on a custom carrier board.  Thanks

  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 8 years ago

    Hi Chase,

    It sounds like you are developing a standalone application?  I ask because I have seen incorrect linker scripts cause the sorts of problems you are describing.  If you have a EV Carrier I would suggest starting with a known-good hardware platform that you can build from our HDL git repository:

    https://github.com/Avnet/hdl

    You will also need the Vivado Board Description File repo:

    https://github.com/Avnet/bdf

    The Vivado build script can be found in the Scripts folder and you run the script by doing the following:

    1.   Open Vivado
    2.   Navigate to the HDL repo Scripts folder in the TCL command window
        cd /path/to/HDL/repo/Scripts
    3.   Start the script
        source ./make_uz_petalinux.tcl

    The script will also build the hardware platforms for the UltraZed-EG SOM and carriers.  You can prevent this by commenting out these lines near the end of the build script.

    This hardware platform is also used to create the PetaLinux BSPs we have posted on this website. 

    http://zedboard.org/support/design/22581/166

    In fact, if you are developing on a Linux host, you can download and install the PetaLinux BSP for the UltraZed-EV and use the Vivado hardware platform that is included in there.  installation instructions for the BSP can be found in Xilinx UG #1144.  The command goes something like this:

    petalinux-create -t project -s ./uz7ev_evcc_2018_2.bsp

    The Vivado project will be found in the extracted uz7ev_evcc_2018_2/hardware/UZ7EV_EVCC folder.

    I hope this helps.

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 8 years ago

    Hi Chase,

    It sounds like you are developing a standalone application?  I ask because I have seen incorrect linker scripts cause the sorts of problems you are describing.  If you have a EV Carrier I would suggest starting with a known-good hardware platform that you can build from our HDL git repository:

    https://github.com/Avnet/hdl

    You will also need the Vivado Board Description File repo:

    https://github.com/Avnet/bdf

    The Vivado build script can be found in the Scripts folder and you run the script by doing the following:

    1.   Open Vivado
    2.   Navigate to the HDL repo Scripts folder in the TCL command window
        cd /path/to/HDL/repo/Scripts
    3.   Start the script
        source ./make_uz_petalinux.tcl

    The script will also build the hardware platforms for the UltraZed-EG SOM and carriers.  You can prevent this by commenting out these lines near the end of the build script.

    This hardware platform is also used to create the PetaLinux BSPs we have posted on this website. 

    http://zedboard.org/support/design/22581/166

    In fact, if you are developing on a Linux host, you can download and install the PetaLinux BSP for the UltraZed-EV and use the Vivado hardware platform that is included in there.  installation instructions for the BSP can be found in Xilinx UG #1144.  The command goes something like this:

    petalinux-create -t project -s ./uz7ev_evcc_2018_2.bsp

    The Vivado project will be found in the extracted uz7ev_evcc_2018_2/hardware/UZ7EV_EVCC folder.

    I hope this helps.

    --Tom