Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EG Starter Kit Sensors Example Design  on vivaldo 2017.2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 255 views
  • Users 0 members are here
Related

UltraZed-EG Starter Kit Sensors Example Design  on vivaldo 2017.2

e14 Contributor
e14 Contributor over 8 years ago

Hi  

I am trying to execute the "UltraZed-EG Starter Kit Sensors Example Design "  written for Vivaldo 2016.4  on Vivaldo 2017.2

When i trying to run the  source ./make_uz_iocc_sensor.tcl   command , the project creation failed with the following errors:

 

WARNING: [IP_Flow 19-4623] Unrecognized family  #.  Please verify spelling and reissue command to set the supported files.

CRITICAL WARNING: [IP_Flow 19-2351] Invalid family lifecycle 'virtex7', should be one of: Beta, Pre-Production, Production, Discontinued, Superseded, Hidden, Removed, Not-Supported
WARNING: [IP_Flow 19-4623] Unrecognized family  Pre-Production.  Please verify spelling and reissue command to set the supported files.
CRITICAL WARNING: [IP_Flow 19-2351] Invalid family lifecycle 'qzynq', should be one of: Beta, Pre-Production, Production, Discontinued, Superseded, Hidden, Removed, Not-Supported
WARNING: [IP_Flow 19-4623] Unrecognized family  Pre-Production.  Please verify spelling and reissue command to set the supported files.
***** Creating Vivado Project...
WARNING: [Device 21-436] No parts matched 'xczu3eg-sfva625-1-i-es1'
ERROR: [Coretcl 2-106] Specified part could not be found.
 
    while executing
"source ./ProjectScripts/$project.tcl -notrace"
    ("UZ3EG_IOCC" arm line 2)
    invoked from within
"switch -nocase $board {
   PZ7015_FMCCC               -
   PZ7030_FMCCC               -
   PZ7010_FMC2                -
   PZ7020_FMC2                ..."
    (file "./make.tcl" line 303)
 
    while executing
"source ./make.tcl -notrace"
    (file "./make_uz_iocc_sensor.tcl" line 52)

 

Where may i find the UltraZed-EG Starter Kit Sensors Example Design  running on Vivaldo 2017.2 , or  some another way to solve the problem

Thanks 

Genady

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Genady,

    That reference designs latest update is to 2016.4. My suggestion would be for you to download Vivado 2016.4 and run the project generation script. If you are dead set on using Vivado 2017.2, my suggestion would be for you to first build the project in 2016.4 and then try to recreate the project from scratch in 2017.2 using the 2016.4 design as a reference.

    --Josh