Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Power fails on AES-ZU3EGES-1-SK-G  boards
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 28 replies
  • Subscribers 365 subscribers
  • Views 3811 views
  • Users 0 members are here
Related

Power fails on AES-ZU3EGES-1-SK-G  boards

100jwilly
100jwilly over 9 years ago

After running I/O carrier board and module for about 4 hours the power to the boards failed.

This has occurred on another board set we using for development. Jumpers on IO carrier boards are in the correct positions and JP1 on SOC module is removed.

Led D10 VIN-HDR is on and led D9 PG-MODULE is off.

Tried cycling the power off and on but will not power up.

Has this been observed on other UltraZed boards? Any way to get this working?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi John,

    Two more questions,

    1) Please measure the +VIN to the SOM. This should be 12V from the carrier. You can measure this at U21 pin 2 or various other caps around the board. C189 – C196. One side is ground, other should be 12V when the carrier is turned on.

    2) Also do you have another SOM to try with the same IO carrier card? Or as I read above, has this issue been replicated on two seperate SOMs?

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi John,

    Two more questions,

    1) Please measure the +VIN to the SOM. This should be 12V from the carrier. You can measure this at U21 pin 2 or various other caps around the board. C189 – C196. One side is ground, other should be 12V when the carrier is turned on.

    2) Also do you have another SOM to try with the same IO carrier card? Or as I read above, has this issue been replicated on two seperate SOMs?

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • 100jwilly
    0 100jwilly over 9 years ago in reply to jafoste4

    Hi Josh,

    12V power to SOM module is present. Measured 12.03V at via connecting 12,13,14 on U19.

    The other IO carrier and SOM is not working, same problem.

    John